SLVUDP6 June 2026 TPS61383-Q1
The J5 jumper is used to enable boost function. By default, this jumper is set to the H2 position, which uses the LDO on the EVM to pull up the EN_BST pin and enable the boost function. Put this jumper in the H1 position to use the USB2ANY adapter to pull up the EN_BST pin and enable boost function. Put this jumper in the L position to disable boost function.