SLVUDK4 December 2025
The TPSM8287B30 EVM GUI is provided on the TPSM8287B30-2X-EVM tool folder to communicate with the device over the I2C bus through the USB2ANY adapter EVM. A valid input voltage must be applied.
The GUI automatically connects to the EVM. If this connection does not happen, then click either the Connect button at the top right of the GUI or the link symbol at the very bottom left of the GUI.