SLVUD71 June 2025
The TPS544B28RBHEVM includes a 10Ω series resistor in the feedback loop for VOUT. The resistor is accessible at the test points TP9, TP10 for loop response analysis. Use these test points during loop response measurements as the perturbation injecting points for the loop. See the description in Table 4-2.
| Test Point | Node Name | Comment |
|---|---|---|
| TP9 | Bode– | Appropriate amplitude of the perturbation is injected across the test points. Bode can be measured by a network analyzer. |
| TP10 | Bode+/Vout_REG |