SLVUBY1 August 2022
Figure 5-1, Figure 5-2, and Figure 5-3 show the board layout for the TPS62932EVM. The top layer contains the main power traces for VIN, VOUT, and ground. Connections for the pins of the TPS62932 and a large area filled with ground are also on the top layer. Most of the signal traces are also located on the top side. The input decoupling capacitors, C6, C7, C8, and C9 are located as close to the IC as possible. The input and output connectors, test points, and all of the components are located on the top side. The bottom layer is a ground plane along with the switching node copper fill, signal ground copper fill, and the feedback trace from the point of regulation to the top of the resistor divider network. Both the top layer and bottom layer use 2-oz copper thickness.
Figure 5-4 and Figure 5-5 are the TPS62932EVM board top view and bottom view, respectively.