SLVK244 January   2026 TRF0213-SEP

 

  1.   1
  2.   2
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects
  6. 3Test Device and Evaluation Board Information
  7. 4Irradiation Facility and Setup
  8. 5Depth, Range, and LETEFF Calculation
  9. 6Test Set-Up and Procedures
  10. 7Single-Event Latch-up (SEL) Results
  11. 8Single-Event Transients (SET) Results
  12. 9Summary
  13.   A Total Ionizing Dose from SEE Experiments
  14.   B References

Total Ionizing Dose from SEE Experiments

The production TRF0213-SEP POL is rated to a total ionizing dose (TID) of 30krad(Si), with information-only data provided up to 50krad(Si). In the course of the SEE testing, the heavy-ion exposures delivered ≈ 1krad(Si) per 106 ions/cm2 run. The cumulative TID exposure for each device respectively, over all runs they each underwent, was determined to be greater than 50krad(Si). The three production TRF0213-SEP devices used in the studies described in this report stayed within specification and were fully-functional after the heavy-ion SEE testing was completed.