SLVK226 October 2025 TPS7H4012-SEP , TPS7H4013-SEP
The TPS7H401x-SEP is packaged in a 44-pin plastic package as shown in Figure 3-1. The TPS7H401x-SEP evaluation module (EVM) was used to evaluate the performance and characteristics of the TPS7H401x-SEP under heavy ion radiation. The TPS7H4012EVM is shown in Figure 3-2 and its EVM schematic is shown in Figure 3-4. The TPS7H4013EVM is shown in Figure 3-3 and its EVM schematic is shown in Figure 3-4.
The package was delidded to reveal the die face for all heavy-ion testing.
Jumper on J6 was configured in the 2-3 position for all testing
Jumper on J6 was configured in the 2-3 position for all testing
Figure 3-5 TPS7H4013EVM Schematics