SLVAFB4 July   2022 TPS62902-Q1 , TPS62903 , TPS62903-Q1

 

  1.   Abstract
  2.   Trademarks
  3. 1Inverting Buck – Boost Topology
    1. 1.1 Concept
    2. 1.2 Output Current Calculations
    3. 1.3 VIN and VOUT Range
  4. 2Digital Pin Configurations
    1. 2.1 Enable Pin
    2. 2.2 MODE/S-CONF Pin
    3. 2.3 Power Good Pin
  5. 3Design Considerations
    1. 3.1 Input Capacitor Selection
    2. 3.2 Output Inductor Selection
    3. 3.3 Stability Limits and Output Capacitor Selection
  6. 4Typical Performance and Waveforms
  7. 5Conclusion
  8. 6References

Input Capacitor Selection

An input capacitor, CIN, is required to provide a local bypass for the input voltage source. A low ESR input capacitor is best for input voltage filtering and minimizing interference with other circuits. For most applications, a 10-µF or 22-μF ceramic capacitor is recommended from VIN to ground. The CIN capacitor value can be increased without any limitation for better input voltage filtering.

For the inverting buck – boost configuration of the TPS62903, it is not recommended to install a capacitor from VIN to - VOUT. Such a capacitor, if installed, provides an AC path from VIN to - VOUT. When VIN is applied to the circuit, this dV/dt across a capacitor from VIN to - VOUT creates a current that must return to ground (the return of the input supply) to complete its loop. This current might flow through the internal low-side MOSFET's body diode and the inductor to return to ground. Flowing through the body diode pulls the SW pin and VOS pin more than 0.3 V below IC ground, violating their absolute maximum rating. Such a condition might damage the TPS62903 and is not recommended. Therefore, a capacitor from VIN to - VOUT is not needed or recommended. If such a capacitor (C_BYP) is present, then a Schottky diode should be installed on the output per Figure 3-1. Startup testing should be conducted to ensure that the SW and VOS pins are not driven more than 0.3 V below IC ground when VIN is applied.

GUID-B445C772-2DAD-4F07-B41D-EA4EA8956579-low.pngFigure 3-1 If Installing C_BYP, Installing Schottky D1 is Required