SLUUCO9A April 2023 – November 2023 BQ28Z620
Class | Subclass | Name | Type | Min | Max | Default | Unit | Description |
---|---|---|---|---|---|---|---|---|
Gas Gauging | IT Cfg | Pack Resistance | I2 | 0 | 32767 | 30 | mΩ | |
Gas Gauging | IT Cfg | System Resistance | I2 | 0 | 32767 | 0 | mΩ | |
Gas Gauging | IT Cfg | Ra Filter | U2 | 0 | 999 | 500 | 0.1% | Filter value used in Ra Updates, specifies what percentage or Ra update is from new value (100%—setting) vs. old value (setting). The recommended setting is 80% if the RSOC_CONV feature is enabled. Otherwise, the setting should be 50% as the default. |
Gas Gauging | IT Cfg | Ra Max Delta | U1 | 0 | 255 | 15 | % of Design Resistance | Maximum value of allowed Ra change |
Gas Gauging | IT Cfg | Reference Grid | UI | 0 | 15 | 4 | Reference Grid point used by Design Resistance. The default setting should be used if RSOC_CONV feature is enabled. Otherwise, grid point 11 should be used to ensure resistance updates fast enough at the grid where discharge termination occurs. | |
Gas Gauging | IT Cfg | Resistance Parameter Filter | U2 | 1 | 65534 | 65124 | — | This is one of the filters used for resistance update. Reducing this filter setting can improve low temperature performance at high rates. The default setting is 41-s time constant. It is recommended to keep this filter within the range of 4 s (that is, DF setting = 61680) up to the default 41 s (that is, DF setting = 65142). Examining the Term Voltage Delta setting and Fast Scale Start SOC should be done prior to twisting this parameter when trying to improve the RSOC performance. The following is the formula to convert the DF setting into actual filter time constant: Filter time constant = [0.25/(1 – (DF_Value /65536))] – 0.25. |
Gas Gauging | IT Cfg | Near EDV Ra Param Filter | U2 | 1 | 65535 | 59220 | — | Ra filter used in the fast scaling region if [FF_NEAR_EDV] = 1. Default value should be used. |
Gas Gauging | IT Cfg | QMax Delta | U1 | 3 | 100 | 5 | % | Maximum allowed QMax change from its previous value. The QMax change will be capped by this setting if the delta from the previous QMax is larger than QMax Delta. QMax Delta is a percentage of Design Capacity. |
Gas Gauging | IT Cfg | QMax Upper Bound | U1 | 100 | 255 | 130 | % | Maximum QMax value over the lifetime of the pack. If the updated QMax value is larger than this setting, the updated QMax will be capped to QMax Upper Bound. QMax Upper Bound is a percentage of Design Capacity. |
Gas Gauging | IT Cfg | Term Voltage | I2 | 0 | 32767 | 9000 | mV | Min stack voltage to be used for capacity calculation |
Gas Gauging | IT Cfg | Term Voltage Delta | I2 | 0 | 32767 | 300 | mV | Controls when the RSOC_CONV feature becomes active. The recommended setting is 3.3 –Term Voltage/Number Cells. The default setting is 300 mV, which is assuming a typical 3-V termination voltage per cell. If a different termination voltage is used, this parameter should be adjusted accordingly. |
Gas Gauging | IT Cfg | Max Simulation Iterations | U1 | 20 | 50 | 30 | The maximum number of iterations allowed for simulation. | |
Gas Gauging | IT Cfg | Term Min Cell Voltage | I2 | 0 | 32767 | 2800 | mV | Minimum cell termination voltage when used, if [CELL_TERM]= 1. This is intended to allow the IT algorithm to reach 0% before CUV is triggered; therefore, this value should be set at or above CUV:Threshold. |
Gas Gauging | IT Cfg | Fast Scale Start SOC | U1 | 0 | 100 | 10 | % | Control start of convergence when [RSOC_CONV]= 1 based on RSOC %. Raising this setting can improve RSOC drop at the end of discharge. However the RSOC % chosen for this setting must keep after the sharp drop of the discharge curve (the knee of the discharge curve). |
Gas Gauging | IT Cfg | Load Select | U1 | 0 | 255 | 7 | Defines Load compensation mode used by the gauging algorithm | |
Gas Gauging | IT Cfg | Load Mode | U1 | 0 | 255 | 0 | Defines unit used by the gauging algorithm: 0 = Constant Current 1 = Constant Power | |
Gas Gauging | IT Cfg | Design Resistance | Averaged cell resistance at Reference Grid point. Automatically updated when Update Status is set to 0x6 by the gauge. To automatically update again, set Update Status to 0x4 or manually set when Update Status is set to 0x6. | |||||
Gas Gauging | IT Cfg | User-Rate-mA | I2 | –32768 | 32768 | 0 | mA | Discharge rate used for capacity calculation selected by Load Select |
Gas Gauging | IT Cfg | User-Rate-mW | I2 | –32768 | 32768 | 0 | 10 mW | Discharge rate used for capacity calculation selected by Load Select |
Gas Gauging | IT Cfg | Reserve Cap-mAh | I2 | 0 | 9000 | 0 | mAh | Capacity is reserved available when the gauging algorithm reports 0% RelativeStateOfCharge(). |
Gas Gauging | IT Cfg | Reserve Cap-cWh | I2 | 0 | 32000 | 0 | cWh | Capacity reserved is available when the gauging algorithm reports 0% RelativeStateOfCharge(). |