SLUAAH3 October 2021 UCC28056
The VOSNS pin monitors output capacitor voltage via an external resistor divider. An internal comparator (OVP1) monitors the VOSNS pin voltage (VOS). If the voltage on this pin rises above VOvp1Rise, indicating excessive output capacitor voltage, then the controller transitions to its BstOffb state. In this state switching halts to prevent further increase in the output voltage. The controller returns to the Runb state, and resumes switching operation, only after VOS falls below VOvp1Fall, indicating that the output voltage has returned to normal range.
The UCC28056A has 108% VOvp1Rise which is less than the UCC28056B (110%) and UCC28056C (110%). The overshoot performance is better when using the UCC28056A, especially during start-up condition. The waveform in Figure 4-2 shows where the controller enters into OVP1.