SLDU007C March 2012 – November 2015
The PGA450Q1EVM runs from the PGA450-Q1 device that is soldered to the board. In addition, the EVM provides a footprint for a socket to enable programming the OTP in devices that are for customer-board use. The socket is not populated by default on the EVM. The part number for the recommended socket is OTS-28-0.65-01.
The GUI then can be used to select the target PGA450-Q1 device when programming OTP (the two options are the soldered device, or the device in the socket). More details of how to do this are described in the OTP section.