SLDU007C March   2012  – November 2015

 

  1.   PGA450Q1EVM User’s Guide
    1.     Trademarks
    2. 1  Read This First
    3. 2  EVM Overview
    4. 3  Power-Supply Requirements and Connections
      1. 3.1 Power Supply
      2. 3.2 Controlling and Powering the PGA450Q1EVM via the USB Interface Board
      3. 3.3 Connecting the Transducer
    5. 4  Jumper Settings
      1. 4.1 Jumpers
      2. 4.2 Default Jumper Settings
      3. 4.3 0-Ω Resistors
    6. 5  Socket for Programming OTP
    7. 6  Transformer and Transducer
    8. 7  PGA450-Q1 Communication Interfaces
      1. 7.1 SPI
      2. 7.2 LIN
      3. 7.3 UART
    9. 8  Controlling the PGA450-Q1 Memory Spaces With the GUI
      1. 8.1 Using the Register Grids to Manipulate the Register Spaces
        1. 8.1.1 ZERO GRID
        2. 8.1.2 DESELECT GRID
        3. 8.1.3 SAVE GRID
        4. 8.1.4 RECALL GRID
        5. 8.1.5 READ SELECTED
        6. 8.1.6 WRITE SELECTED
        7. 8.1.7 READ ALL
        8. 8.1.8 WRITE ALL
      2. 8.2 ESFR Registers
      3. 8.3 EEPROM Registers
        1. 8.3.1 Program EEPROM
        2. 8.3.2 Reload EEPROM
      4. 8.4 RAM
      5. 8.5 OTP
        1. 8.5.1 Load .HEX File Into GUI
        2. 8.5.2 Program OTP Memory from .HEX File
        3. 8.5.3 Verify OTP Programming
        4. 8.5.4 Check OTP Status
      6. 8.6 DEVRAM
      7. 8.7 FIFO/ECHO
        1. 8.7.1 FIFO
        2. 8.7.2 EVAL Monitor
          1. 8.7.2.1 No. of Loops
          2. 8.7.2.2 Trigger
          3. 8.7.2.3 Resolution
          4. 8.7.2.4 Clear Plot
          5. 8.7.2.5 Export Data to Excel
          6. 8.7.2.6 Start/Stop
    10. 9  LIN Master
    11. 10 Keil uVision Settings for Programming Firmware to the PGA450-Q1 DEVRAM or OTP Memory
      1. 10.1 Objective
      2. 10.2 Setup
    12. 11 Use Case
      1. 11.1 Evaluation Through SPI Communication
      2. 11.2 Monitoring the Signal Path
    13. 12 PGA450Q1EVM Schematics and Layout Drawings
  2.   Revision History

Jumpers

Table 1 shows the function of each specific jumper setting on the EVM.

Table 1. Jumpers

Reference Jumper Setting Function
VPWR:VOTP Closed VP_OTP power supply input on the PGA450-Q1 device is connected to the 8-V voltage supply on the EVM.
Open VP_OTP power supply input on the PGA450-Q1 device is not connected to the 8-V voltage supply on the EVM.
VPWR:VLIN Closed VPWR is connected to V_LIN, which is the LIN bus voltage.
Open VPWR is not connected to V_LIN, which is the LIN bus voltage.
JP3 Closed The secondary of the transformer on the EVM is connected to the PGA450-Q1 device on the EVM.
Open The secondary of the transformer on the EVM is not connected to the PGA450-Q1 device on the EVM.
JP4 Closed The transformer primary top terminal is connected to the OUTA pin on the PGA450-Q1 device, for push-pull configuration.(1)
Open The transformer primary top terminal is not connected to the OUTA pin on the PGA450-Q1 device.
JP5 Closed The transformer primary top terminal is connected to the VREG pin on the PGA450-Q1 device, for single-ended configuration.
Open The transformer primary top terminal is not connected to the VREG pin on the PGA450-Q1 device.
The transformer provided with the EVM is push-pull. When using the single-ended configuration, JP4 must be disconnected and JP5 must be closed