SLDU007C March   2012  – November 2015

 

  1.   PGA450Q1EVM User’s Guide
    1.     Trademarks
    2. 1  Read This First
    3. 2  EVM Overview
    4. 3  Power-Supply Requirements and Connections
      1. 3.1 Power Supply
      2. 3.2 Controlling and Powering the PGA450Q1EVM via the USB Interface Board
      3. 3.3 Connecting the Transducer
    5. 4  Jumper Settings
      1. 4.1 Jumpers
      2. 4.2 Default Jumper Settings
      3. 4.3 0-Ω Resistors
    6. 5  Socket for Programming OTP
    7. 6  Transformer and Transducer
    8. 7  PGA450-Q1 Communication Interfaces
      1. 7.1 SPI
      2. 7.2 LIN
      3. 7.3 UART
    9. 8  Controlling the PGA450-Q1 Memory Spaces With the GUI
      1. 8.1 Using the Register Grids to Manipulate the Register Spaces
        1. 8.1.1 ZERO GRID
        2. 8.1.2 DESELECT GRID
        3. 8.1.3 SAVE GRID
        4. 8.1.4 RECALL GRID
        5. 8.1.5 READ SELECTED
        6. 8.1.6 WRITE SELECTED
        7. 8.1.7 READ ALL
        8. 8.1.8 WRITE ALL
      2. 8.2 ESFR Registers
      3. 8.3 EEPROM Registers
        1. 8.3.1 Program EEPROM
        2. 8.3.2 Reload EEPROM
      4. 8.4 RAM
      5. 8.5 OTP
        1. 8.5.1 Load .HEX File Into GUI
        2. 8.5.2 Program OTP Memory from .HEX File
        3. 8.5.3 Verify OTP Programming
        4. 8.5.4 Check OTP Status
      6. 8.6 DEVRAM
      7. 8.7 FIFO/ECHO
        1. 8.7.1 FIFO
        2. 8.7.2 EVAL Monitor
          1. 8.7.2.1 No. of Loops
          2. 8.7.2.2 Trigger
          3. 8.7.2.3 Resolution
          4. 8.7.2.4 Clear Plot
          5. 8.7.2.5 Export Data to Excel
          6. 8.7.2.6 Start/Stop
    10. 9  LIN Master
    11. 10 Keil uVision Settings for Programming Firmware to the PGA450-Q1 DEVRAM or OTP Memory
      1. 10.1 Objective
      2. 10.2 Setup
    12. 11 Use Case
      1. 11.1 Evaluation Through SPI Communication
      2. 11.2 Monitoring the Signal Path
    13. 12 PGA450Q1EVM Schematics and Layout Drawings
  2.   Revision History

LIN Master

The PGA450Q1EVM GUI communicates with the PGA450-Q1 device using LIN. The USB Communication board UART is the LIN master, and the PGA450-Q1 device is the LIN slave. The GUI can be used to configure the LIN frames that are transmitted to the PGA450-Q1 device.

figure9_LIN_master_sdlu007.pngFigure 10. LIN Master on GUI

In order to transmit data to PGA450-Q1 device using a LIN frame, the user must do the following:

  1. Enter the Frame PID in Edit Box corresponding to “Tx Frame PID”. The PID must be entered in hex. Note that valid PID ranges from 0x00 to 0x3F. The GUI software calculates the parity bits using the LIN 2.1 method before the PID is transmitted to the slave.
  2. Enter 0–8 bytes of data in the “Data to be Txed” box. Each data byte must be entered in Hex.
  3. Select the CLASSIC or ENHANCED checksum, which must match the LIN checksum setting in the PGA450-Q1 ESFR LIN_CFG register.
  4. Click on the TRANSMIT button

In order to receive data from PGA450-Q1 device using a LIN frame, the user must do the following:

  1. Enter the Frame PID in Edit Box corresponding to “Rx Frame PID”. The PID must be entered in hex. Note that valid PID ranges from 0x00 to 0x3F. The GUI software calculates the parity bits using the LIN 2.1 method before the PID is transmitted.
  2. Enter the number of data bytes the user expects back from the PGA450-Q1 device.
  3. Select the CLASSIC or ENHANCED checksum
  4. Click on the RECEIVE button

The data received from the PGA450-Q1 device is displayed in the Data Received box.

If the data communication is not working, try Reset This Application, which power-cycles the LIN master IC on the EVM.