SLDU007C March 2012 – November 2015
The 0-Ω resistor R2 is used to connect the programming voltage to the PGA450-Q1 device that is soldered to the PCB. This resistor is not populated on the PCB. The soldered device has had the OTP programmed for DEVRAM usage.
| Reference | Install | Function |
|---|---|---|
| R2 | DNP | The VP_OTP pin of the device does not have OTP programming voltage. |
Although they are installed to default settings in the factory, it is recommended that the user verify that the jumpers and 0-Ω resistors are installed to their default settings before powering on the EVM.