SLAU664B February   2016  – August 2017

 

  1.   MSP430FR2311 LaunchPad™ Development Kit (MSP‑EXP430FR2311)
    1.     Trademarks
    2. 1 Getting Started
      1. 1.1 Introduction
      2. 1.2 Key Features
      3. 1.3 What's Included
        1. 1.3.1 Kit Contents
        2. 1.3.2 Software Examples
      4. 1.4 First Steps: Out-of-Box Experience
        1. 1.4.1 Connecting to the Computer
        2. 1.4.2 Running the Out-of-Box Demo
      5. 1.5 Next Steps: Looking Into the Provided Code
    3. 2 Hardware
      1. 2.1 Block Diagram
      2. 2.2 Hardware Features
        1. 2.2.1 MSP430FR2311 MCU
        2. 2.2.2 eZ-FET Onboard Emulator With EnergyTrace™ Software
        3. 2.2.3 Emulator Connection: Isolation Jumper Block
        4. 2.2.4 Application (or "Backchannel") UART
        5. 2.2.5 Special Features
          1. 2.2.5.1 Smart Analog Combo (SAC)
      3. 2.3 Power
        1. 2.3.1 eZ-FET USB Power
        2. 2.3.2 BoosterPack Plug-In-Module and External Power Supply
      4. 2.4 Measure MSP430 MCU Current Draw
      5. 2.5 Clocking
      6. 2.6 Using the eZ-FET Emulator With a Different Target
      7. 2.7 BoosterPack Plug-in Module Pinout
      8. 2.8 Design Files
        1. 2.8.1 Hardware
        2. 2.8.2 Software
      9. 2.9 Hardware Change log
    4. 3 Software Examples
      1. 3.1 Out-of-Box Software Example
        1. 3.1.1 Source File Structure
        2. 3.1.2 Power Measurement
      2. 3.2 Blink LED Example
        1. 3.2.1 Source File Structure
      3. 3.3 Software I2C Example
        1. 3.3.1 Source File Structure
    5. 4 Resources
      1. 4.1 Integrated Development Environments
        1. 4.1.1 TI Cloud Development Tools
          1. 4.1.1.1 TI Resource Explorer Cloud
          2. 4.1.1.2 Code Composer Studio Cloud
        2. 4.1.2 Code Composer Studio IDE
        3. 4.1.3 IAR Embedded Workbench for Texas Instruments MSP430
        4. 4.1.4 Energia
      2. 4.2 LaunchPad Websites
      3. 4.3 MSPWare Software and TI Resource Explorer
      4. 4.4 FRAM Utilities
      5. 4.5 MSP430FR2311MCU
        1. 4.5.1 Device Documentation
        2. 4.5.2 MSP430FR2311 MCU Code Examples
        3. 4.5.3 MSP430 MCU Application Notes and TI Designs
      6. 4.6 Community Resources
        1. 4.6.1 TI E2E Online Community
        2. 4.6.2 Community-at-Large
    6. 5 FAQ
    7. 6 Schematics
  2.   Revision History

Out-of-Box Software Example

This section describes the functionality and structure of the out-of-box software that is preloaded on the EVM.

This demo shows how to use the op-amp module, combined with the timer, ADC, and LED, to implement a simple light sensor circuit for ultra-low-power applications.

Upon powering up the out-of-box demo, LED1 will toggle at startup and then LED2 will dim based on the amount of ambient light in the area. If the user covers the photo diode, D1, with a piece of paper or their hand the brightness of LED2 should dim based on the amount of light. If the user illuminates the photo diode with a light source LED2 should increase in brightness until the ADC saturates and the LED reaches full brightness. The current ADC reading is saved to FRAM memory before the device re-enters LPM3.