SLAU664B February   2016  – August 2017

 

  1.   MSP430FR2311 LaunchPad™ Development Kit (MSP‑EXP430FR2311)
    1.     Trademarks
    2. 1 Getting Started
      1. 1.1 Introduction
      2. 1.2 Key Features
      3. 1.3 What's Included
        1. 1.3.1 Kit Contents
        2. 1.3.2 Software Examples
      4. 1.4 First Steps: Out-of-Box Experience
        1. 1.4.1 Connecting to the Computer
        2. 1.4.2 Running the Out-of-Box Demo
      5. 1.5 Next Steps: Looking Into the Provided Code
    3. 2 Hardware
      1. 2.1 Block Diagram
      2. 2.2 Hardware Features
        1. 2.2.1 MSP430FR2311 MCU
        2. 2.2.2 eZ-FET Onboard Emulator With EnergyTrace™ Software
        3. 2.2.3 Emulator Connection: Isolation Jumper Block
        4. 2.2.4 Application (or "Backchannel") UART
        5. 2.2.5 Special Features
          1. 2.2.5.1 Smart Analog Combo (SAC)
      3. 2.3 Power
        1. 2.3.1 eZ-FET USB Power
        2. 2.3.2 BoosterPack Plug-In-Module and External Power Supply
      4. 2.4 Measure MSP430 MCU Current Draw
      5. 2.5 Clocking
      6. 2.6 Using the eZ-FET Emulator With a Different Target
      7. 2.7 BoosterPack Plug-in Module Pinout
      8. 2.8 Design Files
        1. 2.8.1 Hardware
        2. 2.8.2 Software
      9. 2.9 Hardware Change log
    4. 3 Software Examples
      1. 3.1 Out-of-Box Software Example
        1. 3.1.1 Source File Structure
        2. 3.1.2 Power Measurement
      2. 3.2 Blink LED Example
        1. 3.2.1 Source File Structure
      3. 3.3 Software I2C Example
        1. 3.3.1 Source File Structure
    5. 4 Resources
      1. 4.1 Integrated Development Environments
        1. 4.1.1 TI Cloud Development Tools
          1. 4.1.1.1 TI Resource Explorer Cloud
          2. 4.1.1.2 Code Composer Studio Cloud
        2. 4.1.2 Code Composer Studio IDE
        3. 4.1.3 IAR Embedded Workbench for Texas Instruments MSP430
        4. 4.1.4 Energia
      2. 4.2 LaunchPad Websites
      3. 4.3 MSPWare Software and TI Resource Explorer
      4. 4.4 FRAM Utilities
      5. 4.5 MSP430FR2311MCU
        1. 4.5.1 Device Documentation
        2. 4.5.2 MSP430FR2311 MCU Code Examples
        3. 4.5.3 MSP430 MCU Application Notes and TI Designs
      6. 4.6 Community Resources
        1. 4.6.1 TI E2E Online Community
        2. 4.6.2 Community-at-Large
    6. 5 FAQ
    7. 6 Schematics
  2.   Revision History

Clocking

The MSP-EXP430FR2311 provides an input for an external clock in addition to the internal clocks in the device. No crystal is populated by default to allow all pins to connect to the BoosterPack header. The user can choose to populate any 32.768 kHz crystal that will fit onto the provided footprint. One option is recommended below:

  • Y1: 32-kHz Epson FC-135R 12.5pF crystal, Part #: X1A0001410014

The 32-kHz crystal allows for lower LPM3 sleep currents than do the other low-frequency clock sources. Therefore, the presence of the crystal allows the full range of low-power modes to be used. If using the external Y1 crystal footprint the user will need to remove the 0-ohm resistors R4 and R5 and populate C2 and C3 with the appropriate tuning capacitors for the crystal that is used.

The internal clocks in the device default to the following configuration:

  • MCLK: DCO at 1 MHz
  • SMCLK: DCO at 1 MHz
  • ACLK: REFO at 32.768 kHz

For more information about configuring internal clocks and using the external oscillators, see the MSP430FR4xx and MSP430FR2xx Family User's Guide.