SLAU646F September 2015 – June 2020
Add the following lines to msp430.dat to enable or modify the specific debug options.
MSP430 low-power debugging
msp430_lowpowerdebug=true
MSP430 programming and erase options for GDB
The BSL or the protected memory can be
unlocked at the start of the session using the msp430_connectaction
keyword.
msp430_connectaction=[unlockbsl] [unlockprotected] [<other connect options>]
If protected memory is unlocked, it is
erased on download if the download erase option is set to erasefactory ,
erasemain , or erasemainandinfo , or if the download
erase option is set to erasesegment and the download image includes
protected memory data.
msp430_loadaction
controls whether a reset is done before or after download and also configures erase options
for download.
msp430_loadaction =[resetbefore] [resetafter] [erasefactory|erasemain|erasemainandinfo|eraseuser|erasesegment] [<other load options>]
Where:
erasefactory = MSP430_Erase(type = ERASE_TOTAL, ...) called at the start of
each download
erasemain =
MSP430_Erase(type = ERASE_MAIN, ...) called at the start of each download
erasemainandinfo = MSP430_Erase(type = ERASE_ALL,
...) called at the start of each download
eraseuser = MSP430_Erase(type = ERASE_USER, ...) called at the start of each
download
erasesegment =
MSP430_Erase(type = ERASE_SEGMENT, ...) called the first time that the segment is written
to during each download
Another optional connect action is to reset or erase on connect:
msp430_connectaction=[reset] [erasefactory|erasemain|erasemainandinfo|eraseuser]
If this line is not present, the default is to not reset or erase on connect.
If the BSL or protected areas are unlocked,
they are erased on connect if the erasefactory or
erasemainandinfo options are set. They are erased on download if the
erasefactory , erasemainandinfo , or erasesegment
options are set and the image includes the BSL or protected segment.
No action is taken on the auto run
or launch options as they are outside the scope of the GDB
agent.
MSP430 verification options for GDB
msp430_loadaction
includes a verify keyword. If this keyword is present, each write to
flash is verified.
msp430_loadaction=[verify]
Add MSP430 breakpoints options for GDB
msp430_default_breakpoint = [software|hardware]
By default, the MSP430 GDB agent uses
software breakpoints (type=BP_SOFTWARE) for all GDB break commands. If a
software breakpoint fails, the GDB agent then attempts to set a hardware (type=BP_CODE)
breakpoint. A hardware breakpoint can be set explicitly using the GDB
hbreak command.
If the
msp430_default_breakpoint option is set to hardware, the
GDB agent uses type BP_CODE for all GDB breakpoints (both break and
hbreak commands).