SLAAE30 July 2021 MSP430FR2355
At this distance, the amplitude from the motion events have shrunk substantially, but the motion is still clear in the wave form and clearly stands out vs the small RMS noise. These motion events were still correctly detected by the MSP430.
Figure 4-5 Adult at 36.5 ft (11.1 m),
speed 1 m/s
Figure 4-6 Child at 36.5 ft (11.1 m),
speed 1 m/s