SLAAE29A January 2023 – December 2025 MSPM0C1105 , MSPM0C1106 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
Customer Secure Code (CSC) is a secure boot solution for MSPM0 devices with hardware isolation mechanism (INITDONE). Figure 3-1illustrates the CSC boot and startup sequence. At BOOTRST, TI ROM boot-code execution commences. After successful boot, boot code issues BOOTDONE. At this point, SYSCTL issues a SYSRST to the device to trigger execution from MAIN flash memory. A MAIN flash program always starts from physical address 0x0004 vector (Reset Handler) after boot code is finished. Depending on the CSCEXISTS configuration in NONMAIN flash BCR, there are two execution flow after BOOTDONE:
A MAIN flash program always starts from physical address 0x0004 after BOOTDONE. As bank swap policy is reset during BOOTRST, so the MAIN flash program always starts without bank swap after BOOTDONE. Bank swap only takes effects after INITDONE when both CSCEXISTS and FLASHBANKSWAPPOLICY enabled in NONMAIN configuration.
For the CSC existing case, CSC is responsible for determining execution bank, memory region protections, secure key initialization into the KEYSTORE, take application program integrity and authenticity verification etc. The device is working in a privileged state with permission configuring those security policies. The INITDONE is issued (by writing to SYSCTL.SECCFG.INITDONE, see device specific technical reference manual for the register definition) at the end of CSC, then SYSCTL issues a second SYSRST and all the security policies listed below take effect during INITDONE and cab not be modified until next BOOTRST:
After INITDONE, the device becomes in unprivileged state, and starts execution from address 0x0004 of MAIN flash again, and the CSC executes a second time. This time, the CSC finds that INITDONE has already been issued previously (this is determined by reading the SYSCTL.SECCFG.SECSTATUS.INITDONE bit) and directly jumps to the main application. See Figure 3-2 for the CSC execution flow in privileged state (pre-INITDONE) and unprivileged state (post-INITDONE).
For more details on boot and startup sequence, see SECURITY chapter of MSPM0 G-Series 80-MHz Microcontrollers Technical Reference Manual (Rev. C).