SLAA871 January 2019 AFE7422 , AFE7444
The DAC38RF82 is an RF DAC that generates the signal of the ACPR performance measurements. When measuring ACPR degradation, the RF DAC outputs a clean 20-MHz long-term evolution (LTE) signal centered at 1907 MHz. The output signal of the DAC first passes through a band-pass filter before being connected to the input of the repeater.
Figure 15 shows the test setup for ACPR degradation. The ACPR of the LTE waveform is measured directly at the output of the DAC and also at the output of the repeater using the spectrum analyzer. The comparative difference in ACPR is the degradation of the LTE waveform due to the repeater.
Figure 15. Test Setup for ACPR Degradation