SLAA457B September 2013 – October 2018 MSP430F5500 , MSP430F5501 , MSP430F5502 , MSP430F5503 , MSP430F5504 , MSP430F5505 , MSP430F5506 , MSP430F5507 , MSP430F5508 , MSP430F5509 , MSP430F5510 , MSP430F5513 , MSP430F5514 , MSP430F5515 , MSP430F5517 , MSP430F5519 , MSP430F5521 , MSP430F5522 , MSP430F5524 , MSP430F5525 , MSP430F5526 , MSP430F5527 , MSP430F5528 , MSP430F5529 , MSP430F5630 , MSP430F5631 , MSP430F5632 , MSP430F5633 , MSP430F5634 , MSP430F5635 , MSP430F5636 , MSP430F5637 , MSP430F5638 , MSP430F5658 , MSP430F5659 , MSP430F6630 , MSP430F6631 , MSP430F6632 , MSP430F6633 , MSP430F6634 , MSP430F6635 , MSP430F6636 , MSP430F6637 , MSP430F6638 , MSP430F6658 , MSP430F6659 , MSP430FG6425 , MSP430FG6426 , MSP430FG6625 , MSP430FG6626
To maintain a consistent user experience, it is important that USB devices adhere to compliance standards. Much of this compliance is driven by the USB silicon and software. The MSP430 device derivatives, running the USB API, have passed USB certification testing for all of the device classes that they support. All certification was performed at MCCI, a test house approved by the USB Implementers Forum (USB-IF).
An output of the USB certification process is a test ID, or TID. Table 2 shows the TIDs for all current MSP430 silicon.
| MSP430 Derivative | Package | TID |
|---|---|---|
| MSP430F552x | PT, RGC, RGZ (QFP, QFN) | 40000973 |
| ZQE (BGA) | 40001139 | |
| MSP430F550x, MSP430F5510 | PT, RGC, RGZ (QFP, QFN)
(Note: F5504 in RGZ is not included in this TID; see the next entry) |
40001138 |
| MSP430F5504 | RGZ (QFN) | 41001138 |
| MSP430F563x, MSP430F663x | PZ (QFP) | 40001250 |
| ZQW (BGA) | 40001442 | |
| MSP430F565x, MSP430F665x | PZ (QFP, QFN) | 40001444 |
| ZQW (BGA) | 40001443 |
All MSP430 devices are certified under a vendor ID (VID) unique to the MSP430 MCU (0x2047), separate from TI's main VID (0x0451).