SLAA126B April 2001 – September 2018 MSP430F149 , MSP430F149 , TLC3544 , TLC3544 , TLC3548 , TLC3548
Figure 4 shows the relationship of the EOC and INT signals more clearly. The EOC signal is active low while the ADC is converting the sampled data. It returns to a high state when the conversion is complete.
INT is active low after the (sample plus conversion) period has finished. INT is cleared when a new sample-and-conversion cycle is initiated by either a falling edge of CS (see Figure 4) or rising edge of FS.
Figure 4. EOC/INT Timing