SFFSB97 April   2026 CD74HC4067-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 DW (SOIC, 24) Package
    2. 2.2 RGY (QFN, 24) Package
    3. 2.3 DGS (VSSOP, 24) Package
    4. 2.4 PW (TSSOP, 24) Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 DW (SOIC, 24) Package
    2. 4.2 RGY (QFN, 24) Package
    3. 4.3 DGS (VSSOP, 24) Package
    4. 4.4 PW (TSSOP, 24) Package
  7. 5Revision History

PW (TSSOP, 24) Package

Figure 4-4 shows the CD74HC4067-Q1 pin diagram for the PW (TSSOP, 24) package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the CD74HC4067-Q1 datasheet.

Figure 4-4 Pin Diagram (PW (TSSOP, 24) Package)
Table 4-14 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
COMMON I/O1There is corruption of the signal passed onto the IX pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I72There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I63There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I54There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I45There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I36There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I27There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I18There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I09There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
S010The address is stuck low. The pin cannot control switch states.B
S111The address is stuck low. The pin cannot control switch states.B
GND12There is no effect on the device. The device operates as normal.D
S313The address is stuck low. The pin cannot control switch states.B
S214The address is stuck low. The pin cannot control switch states.B
E15EN is stuck low. The pin can no longer disable the device without a power down.B
I1516There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1417There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1318There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1219There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1120There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1021There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1922There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1823There is corruption of the signal passed onto the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
VCC24The device is not powered. The device is not functional. Observe that the absolute maximum ratings for all pins of the device are met; otherwise, damage to the device is plausible.A
Table 4-15 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
COMMON I/O1There is corruption of the signal passed onto the IX pin.B
I72There is corruption of the signal passed onto the COMMON pin.B
I63There is corruption of the signal passed onto the COMMON pin.B
I54There is corruption of the signal passed onto the COMMON pin.B
I45There is corruption of the signal passed onto the COMMON pin.B
I36There is corruption of the signal passed onto the COMMON pin.B
I27There is corruption of the signal passed onto the COMMON pin.B
I18There is corruption of the signal passed onto the COMMON pin.B
I09There is corruption of the signal passed onto the COMMON pin.B
S010The address is stuck low. The pin cannot control switch states.B
S111The address is stuck low. The pin cannot control switch states.B
GND12There is no effect on the device. The device operates as normal.A
S313The address is stuck low. The pin cannot control switch states.B
S214The address is stuck low. The pin cannot control switch states.B
E15EN is stuck low. The pin can no longer disable the device without a power down.B
I1516There is corruption of the signal passed onto the COMMON pin.B
I1417There is corruption of the signal passed onto the COMMON pin.B
I1318There is corruption of the signal passed onto the COMMON pin.B
I1219There is corruption of the signal passed onto the COMMON pin.B
I1120There is corruption of the signal passed onto the COMMON pin.B
I1021There is corruption of the signal passed onto the COMMON pin.B
I922There is corruption of the signal passed onto the COMMON pin.B
I823There is corruption of the signal passed onto the COMMON pin.B
VCC24The device is not powered. The device is not functional.B
Table 4-16 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
COMMON I/O1I7There is possible corruption of the signal passed on to the IX pin.B
I72I6There is possible corruption of the signal passed on to the IX and COMMON pin.B
I63I5There is possible corruption of the signal passed on to the IX and COMMON pin.B
I54I4There is possible corruption of the signal passed on to the IX and COMMON pin.B
I45I3There is possible corruption of the signal passed on to the IX and COMMON pin.B
I36I2There is possible corruption of the signal passed on to the IX and COMMON pin.B
I27I1There is possible corruption of the signal passed on to the IX and COMMON pin.B
I18I0There is possible corruption of the signal passed on to the IX and COMMON pin.B
I09S0There is possible corruption of the signal passed on to the IX and COMMON pin.B
S010S1There is possible corruption of the signal passed on to the IX and COMMON pin.B
S111GNDThere is possible damage to the device if the signal voltage is negative. Observe that the absolute maximum ratings for all pins of the device are met; otherwise, damage to the device is possible.B
GND12S3This pin is not considered. This is a corner pin.D
S313S2Control of the address pin is lost. The pin cannot control switch states.B
S214EThere is possible corruption of the signal passed onto the COMMON pin. The switch state is undefined.B
E15I15There is possible corruption of the signal passed onto the COMMON pin. The switch state is undefined.B
I1516I14There is possible corruption of the signal passed on to the IX and COMMON pin.B
I1417I13There is possible corruption of the signal passed on to the IX and COMMON pin.B
I1318I12There is possible corruption of the signal passed on to the IX and COMMON pin.B
I1219I11There is possible corruption of the signal passed on to the IX and COMMON pin.B
I1120I10There is possible corruption of the signal passed on to the IX and COMMON pin.B
I1021I9There is possible corruption of the signal passed on to the IX and COMMON pin.B
I922I8There is possible corruption of the signal passed on to the IX and COMMON pin.B
I823VCCThere is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
VCC24COMMON I/OThis pin is not considered. This is a corner pin.D
Table 4-17 Pin FMA for Device Pins Short-Circuited to Supply
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
COMMON I/O1There is corruption of the signal passed on to the IX pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I72There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I63There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I54There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I45There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I36There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I27There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I18There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I09There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
S010The address is stuck high. The pin cannot control switch states.B
S111The address is stuck high. The pin cannot control switch states.B
GND12The device is not powered and not functional. Observe that the absolute maximum ratings for all pins of the device are met; otherwise, damage to the device is possible.A
S313The address is stuck high. The pin cannot control switch states.B
S214The address is stuck high. The pin cannot control switch states.B
E15EN is stuck high. The pin can no longer enable the device.B
I1516There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1417There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1318There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1219There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1120There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I1021There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I922There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
I823There is corruption of the signal passed on to the COMMON pin. If there is no limiting resistor in the switch path, then device damage is possible.A
VCC24There is no effect on the device. The device operates as normal.D