SFFSAB8 December   2025 TPS7C84-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 SOIC Package
    2. 2.2 VSON Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 SOIC Package
    2. 4.2 VSON Package
  7. 5Revision History

SOIC Package

Figure 4-1 shows the TPS7C84-Q1 pin diagram for the SOIC package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS7C84-Q1 datasheet.

TPS7C84-Q1 Pin Diagram (SOIC) Package Figure 4-1 Pin Diagram (SOIC) Package
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
OUT 1 Regulation of the device is not possible, the device operates at current limit. The device can cycle in an out of thermal shutdown. B
FB/NC 2 (Adjustable) The device operates as a switch in dropout mode. The output tracks the input voltage (VIN) minus the voltage drop out (VDO). B
(Fixed) There is no effect on the device. The device operates normally. D
NC 3 There is no effect on the device. The device operates normally. D
4
GND 5 There is no effect on the device. The device operates normally. D
PG 6 The output of the open drain power good pin is pulled low. C
EN 7 The device is disabled, resulting in no output voltage. B
IN 8 Power is not supplied to the device. System performance depends on limiting the upstream current. B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
OUT 1 The output of the device is disconnected from the load. B
FB/NC 2 (Adjustable) The state of the device is unknown. If the device is on, the output voltage is indeterminate. B
(Fixed) There is no effect on the device. The device operates normally. D
NC 3 There is no effect on the device. The device operates normally. D
4
GND 5 There is no current loop for the supply voltage. The device is not operational and does not regulate. B
PG 6 The output of the open drain power good pin is left floating. C
EN 7 The device potentially does not turn on. B
IN 8 The device is not powered. The device is not functional. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
OUT 1 FB The error amplifier is configured in unity gain:
output voltage = reference voltage.
B
NC (Fixed) There is no effect on the device. The device operates normally. D
FB 2 NC There is no effect on the device. The device operates normally. D
NC 3 NC There is no effect on the device. The device operates normally. D
4
GND 5 PG The output of the open drain power good pin is pulled low. C
PG 6 EN The device remains on. Regulation of the device is possible. C
EN 7 IN The device remains on. Regulation of the device is possible. C
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
OUT 1 Regulation of the device is not possible, leading to an undesired output state. B
FB/NC 2 (Adjustable) The device can have no output voltage. B
(Fixed) There is no effect on the device. The device operates normally. D
NC 3 There is no effect on the device. The device operates normally. D
4
GND 5 Power is not supplied to the device. B
PG 6 There is a loss of the functionality of the PG pin. System-level issues can potentially occur due to unintended current flow in the pullup resistor, depending on the relative magnitudes of the supply voltage and the pullup voltage. A
EN 7 The device remains on. Regulation of the device is possible. C
IN 8 There is no effect on the device. The device operates normally. D