SFFS990 May 2026 UCC27614-Q1
Figure 4-2 and Figure 4-3 show the UCC27614-Q1 pin diagrams for the D (SOIC 8) and DGN (VSSOP 8) packages. For a detailed description of the device pins, see the Pin Configuration and Functions section in the UCC27614-Q1 datasheet.
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VDD | 1 | There is an undervoltage event on the VDD pin. The OUT pin is off. | B |
| IN | 2 | The function of the IN pin is lost. The OUT pin is stuck low. | B |
| EN | 3 | The function of the EN pin is disabled. The OUT pin does not respond to the IN pin. | B |
| GND | 4 | There is no impact to the device. | D |
| GND | 5 | There is no impact to the device. | D |
| OUT | 6 | The OUT pin is stuck low. The OUT pin is shorted if the IN pin is commanded High. | A |
| OUT | 7 | The OUT pin is stuck low. The OUT pin is shorted if the IN pin is commanded High. | A |
| VDD | 8 | There is an undervoltage event on the VDD pin. The OUT pin is off. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VDD | 1 | There is an undervoltage event on the VDD pin. The OUT pin is off. | B |
| IN | 2 | The function of the IN pin is lost. The OUT pin is stuck low. | B |
| EN | 3 | The OUT pin is always enabled. The OUT pin responds to the IN pin. | B |
| GND | 4 | The state of the OUT pin is unknown. | B |
| GND | 5 | The state of the OUT pin is unknown. | B |
| OUT | 6 | The OUT pin is disconnected from the power FET. | B |
| OUT | 7 | The OUT pin is disconnected from the power FET. | B |
| VDD | 8 | There is an undervoltage event on the VDD pin. The OUT pin is off. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| VDD | 1 | IN | The OUT pin is stuck high. | B |
| IN | 2 | EN | The EN pin cannot override the command of the IN pin. The OUT pin responds to the IN pin. | B |
| EN | 3 | GND | The function of the EN pin is disabled. The OUT pin does not respond to the IN pin. | B |
| GND | 5 | OUT | The OUT pin is stuck low. The OUT pin is short circuited if the IN pin is commanded High. | A |
| OUT | 6 | OUT | There is no impact to the device. | D |
| OUT | 7 | VDD | The OUT pin is stuck high. | A |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VDD | 1 | There is no impact to the device. | D |
| IN | 2 | The OUT pin is stuck high. | B |
| EN | 3 | The OUT pin is always enabled. The OUT pin responds to the IN pin. | B |
| GND | 4 | The power supply is short circuited. | B |
| GND | 5 | The power supply is short circuited. | B |
| OUT | 6 | The OUT pin is stuck high. | A |
| OUT | 7 | The OUT pin is stuck high. | A |
| VDD | 8 | There is no impact to the device. | D |