SFFS060 March 2021 DRV8144-Q1
Figure 4-2shows the pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the DRV8144-Q1 data sheet.
Pin | Description of Potential Failure Effect(s) | Failure Effect Class | |
---|---|---|---|
No. | Name | ||
1 | nFAULT | False fault signaling possible. Device will continue to operate as commanded. | B |
2 | IPROPI | IPROPI feedback is lost. ITRIP regulation, if enabled, is also lost. | B |
3 | nSLEEP | Device will be in SLEEP state and OUT is Hi-Z | B |
4 | VM | Device is powered off with driver Hi-Z. | B |
5, 6 | OUT | If OUT is commanded to be pulled high, short is detected and OUT is Hi-Z. | B |
7 | GND | Normal function. | D |
8,9 | OUT | If OUT is commanded to be pulled high, short is detected and OUT is Hi-Z. | B |
10 | VCP | Device damage possible. Device behavior can not be guaranteed. | A |
11 | DRVOFF | Pin based shutoff function is lost. | B |
12 | IN | External PWM control is lost. Internal ITRIP regulation is ok. No risk of spin direction reversal. | B |
13 | nSCS | SPI communication is lost. | B |
14 | SCLK | SPI communication is lost. | B |
15 | SDI | SPI communication is lost. | B |
16 | SDO | SPI communication is lost. | B |
Pin | Description of Potential Failure Effect(s) | Failure Effect Class | |
---|---|---|---|
No. | Name | ||
1 | nFAULT | False fault signaling possible. Device will continue to operate as commanded. | B |
2 | IPROPI | IPROPI feedback is lost. Load will be forced to recirculate if ITRIP regulation is enabled. | B |
3 | nSLEEP | Device will be in SLEEP state and OUT is Hi-Z. | B |
4 | VM | Device is powered off with driver Hi-Z. | B |
5, 6 | OUT | Load drive capability is lost. | B |
7 | GND | Normal function. | D |
8,9 | OUT | Load drive capability is lost. | B |
10 | VCP | The driver can't keep up with PWM frequency > 20 KHz | B |
11 | DRVOFF | Pin based shutoff is triggered and OUT is Hi-Z | B |
12 | IN | External PWM control is lost. Internal ITRIP regulation is OK. No risk of spin direction reversal. | B |
13 | nSCS | SPI communication is lost. | B |
14 | SCLK | SPI communication is lost. | B |
15 | SDI | SPI communication is lost. | B |
16 | SDO | SPI communication is lost. | B |
Short between pins | Description of Potential Failure Effect(s) | Failure Effect Class | |
---|---|---|---|
nFAULT | SDO | False fault signaling possible. SPI communication will be affected during fault assertion. | B |
IPROPI | nFAULT | False fault signaling possible. IPROPI feedback is inaccurate. ITRIP regulation levels, if enabled, will be lower. | B |
nSLEEP | IPROPI | ITRIP regulation levels, if enabled, will be lower. | B |
VM | nSLEEP | SLEEP functionality is lost. | B |
OUT | VM | If OUT is commanded to be pulled low, short is detected and OUT is Hi-Z. | B |
GND | OUT | If OUT is commanded to be pulled high, short is detected and OUT is Hi-Z. | B |
VCP | VM | Pull up path RON (High-side FET) will be much higher. | B |
DRVOFF | VCP | Device damage possible. Device behavior can not be guaranteed. | A |
IN | DRVOFF | Either OUT is Hi-Z or external PWM control is lost. Internal ITRIP regulation is ok. No risk of spin direction reversal. | B |
nSCS | IN | SPI communication is affected. External PWM control is lost. Internal ITRIP regulation is OK. No risk of spin direction reversal. | B |
SCLK | nSCS | SPI communication is lost. | B |
SDI | SCLK | SPI communication is lost. | B |
SDO | SDI | SPI communication is lost. | B |
Pin | Description of Potential Failure Effect(s) | Failure Effect Class | |
---|---|---|---|
No. | Name | ||
1 | nFAULT | Device damage possible. | A |
2 | IPROPI | Device damage possible. | A |
3 | nSLEEP | SLEEP functionality is lost. | B |
4 | VM | Device is powered off with driver Hi-Z. | B |
5, 6 | OUT | If OUT is commanded to be pulled low, short is detected and OUT is Hi-Z. | B |
7 | GND | Normal function. | D |
8,9 | OUT | If OUT is commanded to be pulled low, short is detected and OUT is Hi-Z. | B |
10 | VCP | Pull up path RON (High-side FET) will be much higher. | B |
11 | DRVOFF | OUT is Hi-Z. | B |
12 | IN | Device damage possible. | A |
13 | nSCS | Device damage possible. | A |
14 | SCLK | Device damage possible. | A |
15 | SDI | Device damage possible. | A |
16 | SDO | Device damage possible. | A |