SDAA259 January   2026 AM623 , AM625 , AM625-Q1 , AM625SIP , AM62P , AM62P-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Detailed Description
    1. 2.1 Launching Qt Creator
    2. 2.2 Running The First Project on PC
    3. 2.3 Creating a Button
      1. 2.3.1 Modifying the Property of a Button
    4. 2.4 Creating a C++ Back-End Component
      1. 2.4.1 Defining the Scope of the Project
      2. 2.4.2 Connecting Your C++ Application to Your QML Application
    5. 2.5 Connecting to the EVM
    6. 2.6 Building and Deploying Your Application For Your Embedded Platform
      1. 2.6.1 Build the Application
      2. 2.6.2 Transfer Executable to the Board
    7. 2.7 Running the Application
  6. 3Summary
  7. 4References

Build the Application

To make the build process easier, use a docker image. Here are the steps to build through a docker image. First, cd into the project directory. Use Blink_Tutorial as an example.

Pull TI’s debian-arm64 Docker image and run the image:

docker pull ghcr.io/texasinstruments/debian-arm64:latest

docker run -it -v ${PWD}:/root/workspace ghcr.io/texasinstruments/debian-arm64:latest bash

Inside the container, make the project with the following:

cd /root/workspace

cmake -B build -S .

make -C build

This creates an executable within the build folder that a user can then send to the AM62P.