SDAA195 January 2026 LMG3522R030
In Figure 4-2 and Figure 4-3, waveforms associated with the precharging sequence are provided. The following waveforms are shown:
In this test, the converter under test has been connected to the grid. Note that a grid voltage is present immediately on the terminal of the converter. Once the grid voltage is established a grid inrush current is generated. Voltages across the FETs are effectively clamped to 520V by the zener diodes.