SDAA195 January 2026 LMG3522R030
In a three-level switching cell, the following components can be found as shown in Figure 2-1:
Note that this topology is considered a boost converter topology, where the VSW voltage is always lower than the DC link voltage (VDC).
In this topology, the three voltage levels on the switching node output are achieved by turning the transistors on with the right combination:
As can be seen from the third and fourth switching states, it is important to control the voltages of the two capacitors constant (Vfc and Vdc). This condition makes sure that the switching node voltage is half the DC link voltage, if the flying capacitor voltage is control to half the DC link voltage.