SDAA165 January 2026 TPS61287
Dynamic parameters are related to the switching speed and the energy required to gate driver.
The intrinsic capacitances of a MOSFET (Ciss, Coss, Crss) decide the switching behavior. Figure 2-1 shows the switching process of a usual Boost device low-side MOSFET and then the role of these capacitances is explained.
Figure 2-1 MOSFET Switching WaveformsHow capacitances affect switching speed: when the MOSFET is turning on, the gate driver must charge Ciss (input capacitance) to turn the MOSFET on first (from t0 to t2). As VGS reaches the plateau voltage, the driver current is consumed to discharge Crss, which falls down the VDS (from t2 to t3). A larger total gate charge (Qg) and capacitance require more drive current and time to switch.
Usually there are two negative impacts with larger capacitance:
For controllers with adjustable dead time, the dead time must be set longer than the sum of the turn-off delay of the switch and fall time to avoid shooting-through. While for controllers with fixed dead time like TPS61287, the selected MOSFET must have a sufficiently low Qg or junction capacitance to verify the switching time is shorter than the fixed dead time.
Figure 2-2 Switching Behavior with Poor
Dynamic Characteristic
Figure 2-3 Switching Behavior with Good
Dynamic CharacteristicsFigure 2-2 and Figure 2-3 clearly demonstrates the negative impact of high dynamic parameters on switching speed and the risk of shooting-through.
However, the MOSFET junction capacitance is not as small as possible. Too small a junction capacitance can cause the switching speed to be too fast, increasing the SW voltage spikes (transient voltage at nanosecond level), causing the MOSFET and chip overvoltage stress. For safety of TPS61287, TI recommends that engineers control the voltage spike of the SW below 36V.
Figure 2-4 SW Voltage Spike Measurement with Low-Inductance Probe. If the SW voltage spike is too high due to the selection of a MOSFET with a very small junction capacitance, TI recommends series a drive resistor (RDRV) at the gate of the MOSFET to slow the drive speed and thus reduce the SW voltage spike.
Figure 2-5 Gate Drive Resistor to Slow the Drive Speed and Reduce the SW Voltage Spike