SDAA165 January 2026 TPS61287
This section aims to guide engineers on how to get the input parameters in calculation tool to select a proper MOSFET.
First input the application specifications, entering parameters such as VIN(min/max), VOUT, IOUT, switching frequency and the LC parameters. Then choose a candidate MOSFET and manually enter the key parameters as shown in Figure 3-1.
Figure 3-1 Input MOSFET Parameters in
Calculation ToolThe first parameter in the design calculator is the on-state resistance (RDS(on)). The calculator asks for RDS(on) at 5.1V driving voltage. RDS(on) is typically given in the data sheet either in the electrical characteristics section or in a graph that plots the Vgs versus RDS(on).
The total gate charge (QG) refers to the charge (in coulombs) necessary to charge the gate capacitance to turn on the MOSFET so that the actual gate voltage of the MOSFET matches the driving voltage. This is different from the switching charge. QG is typically given in the MOSFET data sheet.
The internal gate resistance RG can be modeled by a resistor in series with the MOSFET gate, while RG_PCB is the external gate resistance introduced by PCB copper trace or external resistor.
The Ciss, Crss, Coss is the input, reverse and output junction capacitance. Noted that the dynamic characteristic of a MOSFET mainly varies with the drain-source voltage VDS, Figure 3-2 shows the dependency of Ciss, Crss, Coss on VDS. The junction capacitance is typically given in a graph that plots the VDS versus capacitance.
Figure 3-2 MOSFET Ciss,
Crss, Coss versus VDSThe gate-source threshold voltage VGSTH, is the threshold voltage that the MOSFET is turned on, while the gate plateau voltage or miller voltage is the voltage that the Crss is charged. These two voltages are typically given in the MOSFET data sheet.