SCDU019 June   2021

 

  1.   Abstract
  2.   Trademarks
  3. 11. Introduction
    1. 1.1 Information About Cautions and Warnings
  4. 23. Features of This EVM
  5. 34. TMUX741-746EVM Setup
  6. 45. TMUX741-746EVM Jumper Connections and Test Points
  7. 56. Schematics
  8. 67. Bill of Materials
  9. 78. PCB Layouts
  10. 8Related Documentation

4. TMUX741-746EVM Setup

  1. If the default conditions on the board is not what you desired please refer to the following table to set up the Auxiliary pathways which can be either VFP, VFN, SEL, DR, or NC depending on device installed.
    Jumper on Pathway Possible Signal Pull Up Resistor Pad ID Load Resistor Pad ID Load Capacitor Pad ID Additional Capacitor Pad ID
    J7 VFN / SEL R4 R17 C17 C10
    J5 VFN / SEL N/A N/A N/A N/A
    J8 VFP / SEL R6 R18 C18 C9
    J6 VFP / SEL N/A N/A N/A N/A
    J9 DR / SEL R7 R19 C19 N/A
    J10 NC / SEL R8 R20 C20 N/A
  2. If VFP and VFN are used in the application, attach a shunt on J5 and J6 to the appropriate VFP/VFN source.
  3. Next, use the following table to set up the desired configuration of the analog channels:
    Jumper on Pathway Pull Down Resistor Pad ID Pull Up Resistor Pad ID Load Resistor Pad ID Load Capacitor Pad ID TVS Diode Pad ID
    J11 R33 R21 R34 C21 D6
    J12 R35 R22 R36 C22 D7
    J13 R37 R23 R38 C23 D8
    J14 R39 R24 R40 C24 D9
    J15 R53 R41 R54 C25 D10
    J16 R55 R42 R56 C26 D11
    J17 R57 R43 R58 C27 D12
    J18 R59 R44 R60 C28 D13
  4. Next, solder down the chosen TMUX74xx in either a PW or QFN package that is to be tested.
  5. If using dual supplies, connect shunt from VSS to PAD on J19.
  6. If using single supplies, connect shunt from VSS to GND on J4.
  7. Next, power the board through J2. Follow the specific device data sheet as to what range the voltage should be set to.
  8. If VFP/VFN pins are used in the application and are using an external source power this through J3.
  9. If the fault flag voltage (VFF) is used in the application, connect and power up this source through J1.