SBOU327 December 2025
The OPA598EVM ships in a configuration that allows the EVM to be directly applied as an inverting or noninverting amplifier. The jumper shunts as positioned establish the OPA598 as either an inverting amplifier having a gain of –1 V/V when J5 is driven, or a noninverting amplifier having a gain of +2 V/V when J9 is driven. J9 has a 49.9‑Ω, 2-W input terminator connected by a jumper shunt into the input circuit. An external 50-Ω terminator can be placed at the J5 BNC connector when 50-Ω termination is required.
Figure 4-2 shows the default configuration schematic. The complete OPA598 EVM schematic is extensive; therefore, this simplified default schematic is provided to help make the amplifier configuration apparent. See Figure 4-1 for the entire OPA598EVM circuitry and how the Figure 4-2 circuit fits within.
The jumper shunt installations illustrated in Figure 4-2 are designated in the bill of material as a shunt, with an SH-J# part designator. The jumper shunts in Figure 4-2 appear as the red jumpers connected across the various JP# jumper blocks. Arbitrary SH-J# shunt numbers are assigned for this circuit only.