SBOK079 October   2023 TPS7H2140-SEP

PRODUCTION DATA  

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Depth, Range, and LETEFF Calculation
  9. 6 Test Setup and Procedures
  10. 7 Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 8 Single-Event Transients (SET)
  12. 9 Event Rate Calculations
  13. 10Summary
  14. 11References

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product were provided and delivered by the Texas A&M University (TAMU) Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, the ion beams had good flux stability and high irradiation uniformity over a one inch diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For the majority of these studies, ion flux of 105 ions / cm2 × s were used to provide heavy-ion fluences of approximately 107 ions / cm2.

For the experiments conducted in this report, the following ions and corresponding angles were used to provide a range of LETEFF of 48 MeV × cm2 / mg.

  • Silver (109Ag) at 0° for an LETEFF = 48 MeV
    • RangeEFF = 91.2 µm
    • Total Kinetic Energy = 1.634 GeV (15 MeV / nucleon)

Ion uniformity for these experiments was between 93 and 96%.

Figure 4-1 shows the TPS7H2140-SEP test board used for the experiments at the TAMU facility. Although not visible in this photo, the beam port has a 1-mil Aramica window to allow in-air testing while maintaining the vacuum within the accelerator with only minor ion energy loss. The in-air gap between the device and the ion beam port window was maintained at 40 millimeters for all runs.

GUID-20230920-SS0I-HTMM-PH68-1LRBRK0NCH0F-low.jpg Figure 4-1 Photograph of the TPS7H2140-SEP Evaluation Board Mounted in Front of the Heavy-Ion Beam Exit Port at the Texas A&M Cyclotron Radiation Effects Facility