SBOA618 December   2025 TMCS1126

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Current Ratings and Thermal
    1. 2.1 Current Ratings
    2. 2.2 Effects of PCB and Layout
  6. 3Accuracy
  7. 4Bandwidth, Response Time and Propagation Delay
    1. 4.1 Bandwidth
    2. 4.2 Response Time
    3. 4.3 Propagation Delay
  8. 5Lightning and Surge
    1. 5.1 Knowing Lighting and SPD in Solar
    2. 5.2 Understanding IEC 61643-32
    3. 5.3 Understanding IEC 61643-11
    4. 5.4 Surge Requirements in Solar Systems
    5. 5.5 Challenges and Designs for In-Package Hall Sensor
  9. 6Isolation and Reliability
  10. 7Summary
  11. 8References

Propagation Delay

The definition of propagation delay (Tpd) is the period between the input current reaching 10% of the final value and the output voltage reaching 10% of the final value, for an input current step sufficient to cause a 1V change in the output voltage, as shown in Figure 4-2.

Propagation delay is an important parameter during normal operation. For solar applications, average current sampling control is usually used. A large propagation delay can cause the sampling signal to have a big error compared with the real value. As shown in Figure 4-3, the yellow curve is the original input current, red curve is the hall sensor's signal chain output. Although the leading competitor has a higher bandwidth, due to high propagation delay, at the triggering point of ADC sampling, the output of the hall sensor experiences a 1.1us delay compared to the input current. This 1.1us delay causes a large additional offset error when sampling the average value of a triangular current in DC/DC converter. As shown in Figure 4-4, due to a much lower propagation delay, when sampling the average current, this helps minimize the additional offset error, makes the sampling signal chain more accurate.

 Propagation Delay Comparison of Triangular
                        Current Measurement: Leading Competitor: BW Approximately 400kHz, Tprop
                        Approximately 1.1µsFigure 4-3 Propagation Delay Comparison of Triangular Current Measurement: Leading Competitor: BW Approximately 400kHz, Tprop Approximately 1.1µs
 Propagation Delay Comparison of Triangular
                        Current Measurement: TMCS1123: BW Approximately 250kHz, Tprop Approximately
                        0.4µsFigure 4-4 Propagation Delay Comparison of Triangular Current Measurement: TMCS1123: BW Approximately 250kHz, Tprop Approximately 0.4µs

As shown in Figure 4-5, at AC current sampling side, due to the time-varying characteristic of grid voltage (in red curve), the voltage applied to the boost inductor is also changing (in green curve). According to L*di/dt=ΔV, the slew rate of inductor current, di/dt, is time-varying. This varying slew rate causes the additional offset error also be time-varying, as shown in Figure 4-5.

For example, to see the time varying offset error more obviously, in the peak of grid voltage, the slew rate of inductor current is 0.156A/µs, so a 3.2µs total signal chain delay can bring a 0.5A offset to the AC current sensing at the grid voltage peak. But in the middle of grid voltage, the slew rate of inductor current is 0.466A/µs, so a 3.2 µs total delay can bring a 1.5A offset to the AC current sampling result. Figure 4-5 shows a high signal chain delay that brings a big time-varying error to the current loop in AC current sampling.

A time-varying offset error is hard to compensate for, which makes AC output current have worse total harmonic distortion (THD). TI's in-package Hall sensor has a very low propagation delay, which minimizes this time-varying error.

 Time Varying Offset Error with Respect to Slew RateFigure 4-5 Time Varying Offset Error with Respect to Slew Rate

To more intuitively reflect the impact of the time varying offset error, the simulation is done by adding two different Tpd to the feedback of inductor current while keeping other parts of the control loop the same. The current control is a normal PI controller. As shown in Figure 4-6, the inductor current is filtered with a 10kHz low pass filter to lower down the switching frequency ripple and see the current waveform more clearly.

In this example, red curve is with 1us Tpd, inductor current THD(iTHD) is 4.36%. The green curve is with 3us Tpd, iTHD is 4.73%, 0.37% higher than 1us Tpd delay example. It's obvious that a lower propagation delay can decrease the time varying offset error and improve the output current THD. Another point can be observed in the right part of Figure 4-6, is the third harmonic component is 80% lower with a 2us lower Tpd, this helps the converter have a 2% more accurate amplitude in current (0.7A).

 Inductor current with Different Propagation DelaysFigure 4-6 Inductor current with Different Propagation Delays