SBOA618 December 2025 TMCS1126
The definition of response time (Tr) of hall sensor is the period between the input current reaching 90% of the final value and the output voltage reaching 90% of the final value, for an input current step sufficient to cause a 1V change in the output voltage, as shown in Figure 4-2.
In severe short circuit conditions, the slew rate of the current can be very high, so the response time for the current sensor is critical to trigger the short circuit current protection value.
TI's in-package hall-effect current sensor offers the advantage of implementing over-current protection is the dedicated /OC pin which can be used to trigger short circuit protection with only 100ns (typical) delay.