SBAU410 October   2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Overview
    1. 1.1 TMAG5115EVM Kit Contents
    2. 1.2 Related Documentation from Texas Instruments
  4. 2TMAG5115EVM Hardware
  5. 3EVM Operation
    1. 3.1 Quick Start Setup
    2. 3.2 BLDC Motor Operation
      1. 3.2.1 Replacing Sensor Control Board With TMAG5115EVM
      2. 3.2.2 Connecting TMAG5115EVM to a motor driver
      3. 3.2.3 Example Using MCT8316ZTEVM
        1. 3.2.3.1 MCT8316Z Overview
        2. 3.2.3.2 MCT8316ZTEVM Quick Start Guide
        3. 3.2.3.3 Connecting TMAG5115EVM to MCT8316ZTEVM
  6. 4BLDC Motor Manufacturers
  7. 5TMAG5115EVM Circuitry
  8. 6TMAG5115EVM Schematic and PCB Layout
    1. 6.1 Schematic
    2. 6.2 PCB Layout
    3. 6.3 Bill of Materials

Quick Start Setup

  1. Power up the EVM using a variable power supply:
    1. Set the power supply voltage to the desired setting between 3 V and 12 V. Do not turn on the power yet.
    2. Connect the power supply V- terminal to the black GND wire connected to the EVM.
    3. Connect the power supply V+ terminal to the red VCC wire connected to the EVM.
    4. Turn on the power supply
  2. At power up, the device default state is high and the LEDs stay in the off state. Place the handheld D3X8 magnet over one of the three TMAG5115 devices found on the EVM. Depending on the polarity of the magnet, you may see the LED turn on or remain in the off state.
  3. Rotate the magnet to the opposite orientation. If the threshold is met, the device should have the opposing reaction than it did in the previous step. A South field over the BOP will turn on the LED while a North field less than the BRP threshold will turn off the LED. See Figure 3-1 for the magnetic response of a Hall-effect latch.
GUID-CEF4C012-E075-4EB6-B814-ECD5001A3C3B-low.gif Figure 3-1 Hall Latch Output.