SBAA783 January 2026 ISOM8600 , ISOM8610
One important consideration for design is the VOFF of the output when driving a relay or an inductive load. The ISOM8600 supports up to VOFF = 80VDC, however, the free-wheeling voltage (or back EMF) when the ISOM8600 output stops driving the relay coil can cause a transient up to 150VPK. Therefore, additional protection is needed to resolve this challenge.
The energy from the 24V supply is stored in the mechanical relay coil while the output (P1 and P2) is ON. The back EMF is the released coil energy that appears at pin 4 when the output (P1 and P2) switches OFF.
Two common mechanical relays were selected to test the circuit in Figure 2-1 to demonstrate this challenge. The first test shows the free-wheeling voltage generated from the mechanical relay.