SBAA783 January 2026 ISOM8600 , ISOM8610
The input side of the ISOM86x0 is current-driven. As shown in Figure 1-2, a user can place RLIM in series with the input to limit the current flowing into AN pin. RLIM is selected to set the input current ON threshold according to the Recommended Operating Conditions (0.8mA to 20mA) for the ISOM8600.
The equation to calculate RIN for a given input voltage (VIN) and desired input forward current (IF) is shown in Equation 1 where VF is the maximum specification for the ISOM8610 input forward voltage: