ZHCSP86E May 2020 – February 2024 UCC5350-Q1
PRODUCTION DATA
Figure 11-1 shows a PCB layout example with the signals and key components labeled. The UCC5390ECDWV evaluation module (EVM) is given as an example, available in the same DWV package as the UCC5350-Q1. The UCC5390EC has a split emitter versus Miller clamp so although the layout is not exactly the same, general guidelines and practices still apply. The evaluation board can be configured for the Miller clamp version, as well, as described in the UCC5390ECDWV Isolated Gate Driver Evaluation Module User's Guide.
Figure 11-2 and Figure 11-3 show the top and bottom layer traces and copper.
Figure 11-4 shows the 3D layout of the top view of the PCB.