ZHCSDY5C July 2015 – July 2024 TUSB4041I-Q1
PRODUCTION DATA

| PIN | I/O(1) | TYPE(1) | DESCRIPTION | |||||||
|---|---|---|---|---|---|---|---|---|---|---|
| NAME | NO. | |||||||||
| CLOCK AND RESET SIGNALS | ||||||||||
| GRSTz | 18 | I | PU | Global power reset. This reset brings all of the TUSB4041I-Q1 device internal registers to the default state. When the GRSTz pin is asserted, the device is completely nonfunctional. | ||||||
| XI | 30 | I | — | Crystal input. This pin is the crystal input for the internal oscillator. The input can alternately be driven by the output of an external oscillator. When using a crystal, a 1-MΩ feedback resistor is required between the XI and XO pins. | ||||||
| XO | 29 | O | — | Crystal output. This pin is the crystal output for the internal oscillator. If the XI pin is driven by an external oscillator, this pin can be left unconnected. When using a crystal, a 1-MΩ feedback resistor is required between the XI and XO pins. | ||||||
| USB UPSTREAM SIGNALS | ||||||||||
| USB_DM_UP | 22 | I/O | — | USB high-speed differential transceiver (negative) | ||||||
| USB_DP_UP | 21 | I/O | — | USB high-speed differential transceiver (positive) | ||||||
| USB_R1 | 32 | I | — | Precision resistor reference. Connect a 9.53-kΩ ±1% resistor between the USB_R1 pin and ground. | ||||||
| USB_VBUS | 16 | I | — | USB upstream port power monitor. The VBUS detection requires a voltage divider. The signal USB_VBUS must be connected to VBUS through a 90.9-kΩ ±1% resistor and to ground through a 10-kΩ ±1% resistor from the signal to ground. | ||||||
| USB DOWNSTREAM SIGNALS | ||||||||||
| OVERCUR1z | 14 | I | PU | USB port 1 overcurrent detection. This pin is used to connect the overcurrent output of the downstream port power switch for port 1. | ||||||
| 0 = An overcurrent event occurred. | ||||||||||
| 1 = An overcurrent event has not occurred. | ||||||||||
| This pin can be left unconnected if power management is not implemented. If power management is enabled, review the power switch to determine the necessary external circuitry. | ||||||||||
| OVERCUR2z | 15 | I | PU | USB port 2 overcurrent detection. This pin is used to connect the overcurrent output of the downstream port power switch for port 2. | ||||||
| 0 = An overcurrent event occurred. | ||||||||||
| 1 = An overcurrent event has not occurred. | ||||||||||
| If power management is not implemented, leave this pin unconnected. If power management is enabled, review the power switch to determine the necessary external circuitry. | ||||||||||
| OVERCUR3z | 12 | I | PU | USB port 3 overcurrent detection. This pin is used to connect the overcurrent output of the downstream port power switch for port 3. | ||||||
| 0 = An overcurrent event occurred. | ||||||||||
| 1 = An overcurrent event has not occurred. | ||||||||||
| This pin can be left unconnected if power management is not implemented. If power management is enabled, review the power switch to determine the necessary external circuitry. | ||||||||||
| OVERCUR4z | 11 | I | PU | USB port 4 overcurrent detection. This pin is used to connect the overcurrent output of the downstream port power switch for port 4. | ||||||
| 0 = An overcurrent event occurred. | ||||||||||
| 1 = An overcurrent event has not occurred. | ||||||||||
| This pin can be left unconnected if power management is not implemented. If power management is enabled, review the power switch to determine the necessary external circuitry. | ||||||||||
| PWRCTL1/BATEN1 | 4 | I/O | PD | USB port 1 power-on control for downstream power and battery charging enable. The pin is used for control of the downstream power switch for port 1. | ||||||
| The value of the pin is sampled at the deassertion of reset to determine the value of the battery charging support for port 1 as indicated in the Battery Charging Support Register: | ||||||||||
| 0 = Battery charging not supported | ||||||||||
| 1 = Battery charging supported | ||||||||||
| PWRCTL2/BATEN2 | 3 | I/O | PD | USB port 2 power-on control for downstream power and battery charging enable. The pin is used for control of the downstream power switch for port 2. | ||||||
| The value of the pin is sampled at the deassertion of reset to determine the value of the battery charging support for Port 2 as indicated in the Battery Charging Support Register: | ||||||||||
| 0 = Battery charging not supported | ||||||||||
| 1 = Battery charging supported | ||||||||||
| PWRCTL3/BATEN3 | 1 | I/O | PD | USB port 3 power-on control for downstream power and battery charging enable. The pin is used for control of the downstream power switch for port 3. | ||||||
| The value of the pin is sampled at the deassertion of reset to determine the value of the battery charging support for Port 3 as indicated in the Battery Charging Support Register: | ||||||||||
| 0 = Battery charging not supported | ||||||||||
| 1 = Battery charging supported | ||||||||||
| PWRCTL4/BATEN4 | 64 | I/O | PD | USB port 4 power-on control for downstream power and battery charging enable. The pin is used for control of the downstream power switch for port 4. | ||||||
| The value of the pin is sampled at the deassertion of reset to determine the value of the battery charging support for Port 4 as indicated in the Battery Charging Support Register: | ||||||||||
| 0 = Battery charging not supported | ||||||||||
| 1 = Battery charging supported | ||||||||||
| USB_DM_DN1 | 34 | I/O | — | USB high-speed differential transceiver (negative) | ||||||
| USB_DM_DN2 | 42 | |||||||||
| USB_DM_DN3 | 50 | |||||||||
| USB_DM_DN4 | 57 | |||||||||
| USB_DP_DN1 | 33 | I/O | — | USB high-speed differential transceiver (positive) | ||||||
| USB_DP_DN2 | 41 | |||||||||
| USB_DP_DN3 | 49 | |||||||||
| USB_DP_DN4 | 56 | |||||||||
| I2C AND SMBus SIGNALS | ||||||||||
| SCL/SMBCLK | 6 | I/O | PD | I2C clock/SMBus clock. The function of this pin depends on the setting of the SMBUSz input. | ||||||
| When SMBUSz = 1, this pin functions as the serial clock interface for an I2C EEPROM. | ||||||||||
| When SMBUSz = 0, this pin functions as the serial clock interface for an SMBus host. | ||||||||||
| This pin can be left unconnected if external interface not implemented. | ||||||||||
| SDA/SMBDAT | 5 | I/O | PD | I2C data/SMBus data. The function of this pin depends on the setting of the SMBUSz input. | ||||||
| When SMBUSz = 1, this pin functions as the serial data interface for an I2C EEPROM. | ||||||||||
| When SMBUSz = 0, this pin functions as the serial data interface for an SMBus host. | ||||||||||
| This pin can be left unconnected if the external interface is not implemented. | ||||||||||
| SMBUSz | 7 | I/O | PU | I2C/SMBus mode select. The value of the pin is sampled at the deassertion of reset set I2C or SMBus mode as follows: | ||||||
| 1 = I2C mode selected | ||||||||||
| 0 = SMBus mode selected | ||||||||||
| This pin can be left unconnected if the external interface is not implemented. | ||||||||||
| After reset, this signal is driven low by the TUSB4041I-Q1. Because of this behavior, TI recommends not to tie directly to supply, but instead pull up or pull down using external resistor. | ||||||||||
| TEST AND MISCELLANEOUS SIGNALS | ||||||||||
| AUTOENz/ HS_SUSPEND | 13 | I/O | PU | Automatic charge mode enable/HS suspend status | ||||||
| The value of the pin is sampled at the deassertion of reset to determine if automatic mode is enabled as follows: | ||||||||||
| 0 = Automatic mode is enabled on ports that are enabled for battery charging when the hub is unconnected. Note that CDP is not supported on port 1 when operating in automatic mode. | ||||||||||
| 1 = Automatic mode is disabled. | ||||||||||
| This value is also used to set the autoEnz bit in the Battery Charging Support Register. | ||||||||||
| After reset, this signal indicates the high-speed USB Suspend status of the upstream port if enabled through the Additional Feature Configuration Register. When enabled, a value of 1 indicates the connection is suspended. | ||||||||||
| FULLPWRMGMTz/ SMBA1 | 8 | I/O | PD | Full power management enable/SMBus address bit 1 | ||||||
| The value of the pin is sampled at the deassertion of reset to set the power switch control follows: | ||||||||||
| 0 = Power switching and overcurrent inputs supported | ||||||||||
| 1 = Power switching and overcurrent inputs not supported | ||||||||||
| Full power management is the ability to control power to the downstream ports of the TUSB4041I-Q1 device using PWRCTL[4:1]/BATEN[4:1]. | ||||||||||
| When SMBus mode is enabled using SMBUSz, this pin sets the value of the SMBus target address bit 1. | ||||||||||
| This pin can be left unconnected if full power management and SMBus are not implemented. | ||||||||||
| After reset, this signal is driven low by the TUSB4041I-Q1. Because of this behavior, TI recommends not to tie directly to supply, but instead pull up or pull down using an external resistor. | ||||||||||
| Note: Power switching must be supported for battery charging applications. | ||||||||||
| GANGED/SMBA2/ HS_UP | 10 | I/O | PD | Ganged operation enable/SMBus address bit 2/HS connection status upstream port | ||||||
| The value of the pin is sampled at the deassertion of reset to set the power switch and overcurrent detection mode as follows: | ||||||||||
| 0 = Individual power control supported when power switching is enabled | ||||||||||
| 1 = Power control gangs supported when power switching is enabled | ||||||||||
| When SMBus mode is enabled using SMBUSz, this pin sets the value of the SMBus target address bit 2. | ||||||||||
| After reset, this signal indicates the high-speed USB connection status of the upstream port if enabled through the Additional Feature Configuration Register. When enabled, a value of 1 indicates the upstream port is connected to a high-speed USB capable port. | ||||||||||
| Note: Individual power control must be enabled for battery charging applications. | ||||||||||
| PWRCTL_POL | 9 | I/O | PU | Power control polarity. | ||||||
| The value of the pin is sampled at the deassertion of reset to set the polarity of PWRCTL[4:1]. | ||||||||||
| 0 = PWRCTL polarity is active low | ||||||||||
| 1 = PWRCTL polarity is active high | ||||||||||
| RSVD | 23, 24, 26, 27, 35, 36, 38, 39, 43, 44, 46, 47, 51, 52, 54, 55, 58, 59, 61, 62 | I/O | Reserved. For internal use only and leave unconnected on the PCB. | |||||||
| TEST | 17 | I | PD | This pin is reserved for factory test. | ||||||
| POWER AND GROUND SIGNALS | ||||||||||
| NC | 28 | — | — | No connection, leave floating | ||||||
| 40 | ||||||||||
| VDD | 19 | — | PWR | 1.1-V power rail | ||||||
| 25 | ||||||||||
| 37 | ||||||||||
| 45 | ||||||||||
| 53 | ||||||||||
| 60 | ||||||||||
| 63 | ||||||||||
| VDD33 | 2 | — | PWR | 3.3-V power rail | ||||||
| 20 | ||||||||||
| 31 | ||||||||||
| 48 | ||||||||||
| Thermal Pad | — | — | Ground. The thermal pad must be connected to ground. | |||||||