ZHCSN51K June 2007 – June 2024 TPS74901
PRODUCTION DATA
Knowing the device power dissipation and proper sizing of the thermal plane that is connected to the tab or pad is critical to avoiding thermal shutdown and ensuring reliable operation.
Power dissipation of the device depends on input voltage and load conditions, and can be calculated using Equation 4:
Power dissipation can be minimized and greater efficiency can be achieved by using the lowest possible input voltage necessary to achieve the required output voltage regulation.
On the VQFN (RGW) package, the primary conduction path for heat is through the exposed pad to the PCB. The pad can be connected to ground or left floating; however, the pad must be attached to an appropriate amount of copper PCB area to ensure the device does not overheat. On the DDPAK (KTW) package, the primary conduction path for heat is through the tab to the PCB. Connect that tab to ground. The maximum junction-to-ambient thermal resistance depends on the maximum ambient temperature, maximum device junction temperature, and power dissipation of the device and can be estimated using Equation 5:
Knowing the maximum RθJA, the minimum amount of PCB copper area needed for appropriate heat sinking can be estimated using Figure 7-7.

Figure 7-7 shows the variation of RθJA as a function of ground plane copper area in the board. Figure 7-7 is intended only as a guideline to demonstrate the affects of heat spreading in the ground plane; do not use Figure 7-7 to estimate actual thermal performance in real application environments.
When the device is mounted on an application PCB, TI strongly recommends using ΨJT and ΨJB, as explained in the Thermal Considerations section.