ZHCSPX3A October 2022 – November 2022 TMUX7436F
PRODMIX
The on-resistance of the TMUX7436F is the ohmic resistance across the source (Sx) and drain (Dx) pins of the device. The on-resistance varies with input voltage and supply voltage. The symbol RON is used to denote on-resistance. Figure 7-1 shows the measurement setup used to measure RON. ΔRON represents the difference between the RON of any two channels, while RON_FLAT denotes the flatness that is defined as the difference between the maximum and minimum value of on-resistance measured over the specified analog signal range.
Figure 7-1 On-Resistance Measurement Setup