4.1 Device Configuration at Device Reset
Table 4-1 describes the device configuration pins. The logic level is latched at power-on reset to determine the device configuration. The logic level on the device configuration pins can be set by using external pullup/pulldown resistors or by using some control device (e.g., FPGA/CPLD) to intelligently drive these pins. When using a control device, care should be taken to ensure there is no contention on the lines when the device is out of reset. The device configuration pins are sampled during power-on reset and are driven after the reset is removed. To avoid contention, the control device must stop driving the device configuration pins of the DSP. And when driving by a control device, the control device must be fully powered and out of reset itself and driving the pins before the DSP can be taken out of reset.
Also, please note that most of the device configuration pins are shared with other function pins (LENDIAN/GPIO[0], BOOTMODE[12:0]/GPIO[13:1], PCIESSMODE[1:0]/GPIO[15:14] and PCIESSEN/TIMI0), some time must be given following the rising edge of reset in order to drive these device configuration input pins before they assume an output state (those GPIO pins should not become outputs during boot). Another caution that needs to be noted is that systems using TIMI0 (pin shared with PCIESSEN) as a clock input must assure that the clock itself is disabled from the input until after reset is released and a control device is no longer driving that input.
NOTE
If a configuration pin must be routed out from the device and it is not driven (Hi-Z state), the internal pullup/pulldown (IPU/IPD) resistor should not be relied upon. TI recommends the use of an external pullup/pulldown resistor. For more detailed information on pullup/pulldown resistors and situations in which external pullup/pulldown resistors are required, see Section 4.4.
Table 4-1 C6654 Device Configuration Pins
| CONFIGURATION PIN |
PIN NO. |
IPD/IPU(1) |
FUNCTIONAL DESCRIPTION |
| LENDIAN(1)(2) |
T25 |
IPU |
Device endian mode (LENDIAN).
- 0 = Device operates in big endian mode
- 1 = Device operates in little endian mode
|
| BOOTMODE[12:0](1)(2) |
R25, R3, U25, T23, U24, T22, R21, U22, U23, V23, U21, T21, V22 |
IPD |
Method of boot. Some pins may not be used by bootloader and can be used as general purpose config pins. Refer to the Bootloader for the C66x DSP User's Guide (SPRUGY5) for how to determine the device enumeration ID value.
|
| PCIESSMODE[1:0](1)(2) |
W21, V21 |
IPD |
PCIe Subsystem mode selection.
- 00 = PCIe in end point mode
- 01 = PCIe legacy end point (support for legacy INTx)
- 10 = PCIe in root complex mode
- 11 = Reserved
|
| PCIESSEN(1)(2) |
AD20 |
IPD |
PCIe subsystem enable/disable.
- 0 = PCIE Subsystem is disabled
- 1 = PCIE Subsystem is enabled
|
(1) Internal 100-µA pulldown or pullup is provided for this terminal. In most systems, a 1-kΩ resistor can be used to oppose the IPD/IPU. For more detailed information on pulldown/pullup resistors and situations in which external pulldown/pullup resistors are required, see
Section 4.4.
(2) These signal names are the secondary functions of these pins.
4.2 Peripheral Selection After Device Reset
Several of the peripherals on the C6654 are controlled by the Power Sleep Controller (PSC). By default, the PCIe is held in reset and clock-gated. The memory in this module is also in a low-leakage sleep mode. Software is required to turn this memory on. The software enables the module (turns on clocks and de-asserts reset) before this module can be used.
If one of the above modules is used in the selected ROM boot mode, the ROM code will automatically enable the module.
All other modules come up enabled by default and there is no special software sequence to enable. For more detailed information on the PSC usage, see the Power Sleep Controller (PSC) for KeyStone Devices User's Guide (SPRUGV4).
4.3 Device State Control Registers
The C6654 device has a set of registers that are used to provide the status or configure certain parts of its peripherals. These registers are shown in Table 4-2.
Table 4-2 Device State Control Registers
| ADDRESS START |
ADDRESS END |
SIZE |
FIELD |
DESCRIPTION |
| 0x02620000 |
0x02620007 |
8B |
Reserved |
|
| 0x02620008 |
0x02620017 |
16B |
Reserved |
|
| 0x02620018 |
0x0262001B |
4B |
JTAGID |
See Section 4.3.3 |
| 0x0262001C |
0x0262001F |
4B |
Reserved |
|
| 0x02620020 |
0x02620023 |
4B |
DEVSTAT |
See Section 4.3.1 |
| 0x02620024 |
0x02620037 |
20B |
Reserved |
|
| 0x02620038 |
0x0262003B |
4B |
KICK0 |
See Section 4.3.4 |
| 0x0262003C |
0x0262003F |
4B |
KICK1 |
| 0x02620040 |
0x02620043 |
4B |
DSP_BOOT_ADDR0 |
The boot address for C66x DSP CorePac0 |
| 0x02620044 |
0x02620047 |
4B |
Reserved |
Reserved |
| 0x02620048 |
0x0262004B |
4B |
Reserved |
|
| 0x0262004C |
0x0262004F |
4B |
Reserved |
|
| 0x02620050 |
0x02620053 |
4B |
Reserved |
|
| 0x02620054 |
0x02620057 |
4B |
Reserved |
|
| 0x02620058 |
0x0262005B |
4B |
Reserved |
|
| 0x0262005C |
0x0262005F |
4B |
Reserved |
|
| 0x02620060 |
0x026200DF |
128B |
Reserved |
|
| 0x026200E0 |
0x0262010F |
48B |
Reserved |
|
| 0x02620110 |
0x02620117 |
8B |
MACID |
See Section 8.16 |
| 0x02620118 |
0x0262012F |
24B |
Reserved |
|
| 0x02620130 |
0x02620133 |
4B |
LRSTNMIPINSTAT_CLR |
See Section 4.3.6 |
| 0x02620134 |
0x02620137 |
4B |
RESET_STAT_CLR |
See Section 4.3.8 |
| 0x02620138 |
0x0262013B |
4B |
Reserved |
|
| 0x0262013C |
0x0262013F |
4B |
BOOTCOMPLETE |
See Section 4.3.9 |
| 0x02620140 |
0x02620143 |
4B |
Reserved |
|
| 0x02620144 |
0x02620147 |
4B |
RESET_STAT |
See Section 4.3.7 |
| 0x02620148 |
0x0262014B |
4B |
LRSTNMIPINSTAT |
See Section 4.3.5 |
| 0x0262014C |
0x0262014F |
4B |
DEVCFG |
See Section 4.3.2 |
| 0x02620150 |
0x02620153 |
4B |
PWRSTATECTL |
See Section 4.3.10 |
| 0x02620154 |
0x02620157 |
4B |
Reserved |
|
| 0x02620158 |
0x0262015B |
4B |
SMGII_SERDES_STS |
See Section 9.2 |
| 0x0262015C |
0x0262015F |
4B |
PCIE_SERDES_STS |
| 0x02620160 |
0x02620163 |
4B |
Reserved |
|
| 0x02620164 |
0x02620167 |
4B |
Reserved |
|
| 0x02620168 |
0x0262016B |
4B |
Reserved |
|
| 0x0262016C |
0x0262016F |
4B |
UPP_CLOCK |
See Section 4.3.22 |
| 0x02620170 |
0x02620183 |
20B |
Reserved |
|
| 0x02620184 |
0x0262018F |
12B |
Reserved |
|
| 0x02620190 |
0x02620193 |
4B |
Reserved |
|
| 0x02620194 |
0x02620197 |
4B |
Reserved |
|
| 0x02620198 |
0x0262019B |
4B |
Reserved |
|
| 0x0262019C |
0x0262019F |
4B |
Reserved |
|
| 0x026201A0 |
0x026201A3 |
4B |
Reserved |
|
| 0x026201A4 |
0x026201A7 |
4B |
Reserved |
|
| 0x026201A8 |
0x026201AB |
4B |
Reserved |
|
| 0x026201AC |
0x026201AF |
4B |
Reserved |
|
| 0x026201B0 |
0x026201B3 |
4B |
Reserved |
|
| 0x026201B4 |
0x026201B7 |
4B |
Reserved |
|
| 0x026201B8 |
0x026201BB |
4B |
Reserved |
|
| 0x026201BC |
0x026201BF |
4B |
Reserved |
|
| 0x026201C0 |
0x026201C3 |
4B |
Reserved |
|
| 0x026201C4 |
0x026201C7 |
4B |
Reserved |
|
| 0x026201C8 |
0x026201CB |
4B |
Reserved |
|
| 0x026201CC |
0x026201CF |
4B |
Reserved |
|
| 0x026201D0 |
0x026201FF |
48B |
Reserved |
|
| 0x02620200 |
0x02620203 |
4B |
NMIGR0 |
See Section 4.3.11 |
| 0x02620204 |
0x02620207 |
4B |
Reserved |
|
| 0x02620208 |
0x0262020B |
4B |
Reserved |
|
| 0x0262020C |
0x0262020F |
4B |
Reserved |
|
| 0x02620210 |
0x02620213 |
4B |
Reserved |
|
| 0x02620214 |
0x02620217 |
4B |
Reserved |
|
| 0x02620218 |
0x0262021B |
4B |
Reserved |
|
| 0x0262021C |
0x0262021F |
4B |
Reserved |
|
| 0x02620220 |
0x0262023F |
32B |
Reserved |
|
| 0x02620240 |
0x02620243 |
4B |
IPCGR0 |
See Section 4.3.12 |
| 0x02620244 |
0x02620247 |
4B |
Reserved |
|
| 0x02620248 |
0x0262024B |
4B |
Reserved |
|
| 0x0262024C |
0x0262024F |
4B |
Reserved |
|
| 0x02620250 |
0x02620253 |
4B |
Reserved |
|
| 0x02620254 |
0x02620257 |
4B |
Reserved |
|
| 0x02620258 |
0x0262025B |
4B |
Reserved |
|
| 0x0262025C |
0x0262025F |
4B |
Reserved |
|
| 0x02620260 |
0x0262027B |
28B |
Reserved |
|
| 0x0262027C |
0x0262027F |
4B |
IPCGRH |
See Section 4.3.14 |
| 0x02620280 |
0x02620283 |
4B |
IPCAR0 |
See Section 4.3.13 |
| 0x02620284 |
0x02620287 |
4B |
Reserved |
|
| 0x02620288 |
0x0262028B |
4B |
Reserved |
|
| 0x0262028C |
0x0262028F |
4B |
Reserved |
|
| 0x02620290 |
0x02620293 |
4B |
Reserved |
|
| 0x02620294 |
0x02620297 |
4B |
Reserved |
|
| 0x02620298 |
0x0262029B |
4B |
Reserved |
|
| 0x0262029C |
0x0262029F |
4B |
Reserved |
|
| 0x026202A0 |
0x026202BB |
28B |
Reserved |
|
| 0x026202BC |
0x026202BF |
4B |
IPCARH |
See Section 4.3.15 |
| 0x026202C0 |
0x026202FF |
64B |
Reserved |
|
| 0x02620300 |
0x02620303 |
4B |
TINPSEL |
See Section 4.3.16
See Section 4.3.17
|
| 0x02620304 |
0x02620307 |
4B |
TOUTPSEL |
| 0x02620308 |
0x0262030B |
4B |
RSTMUX0 |
See Section 4.3.18 |
| 0x0262030C |
0x0262030F |
4B |
Reserved |
|
| 0x02620310 |
0x02620313 |
4B |
Reserved |
|
| 0x02620314 |
0x02620317 |
4B |
Reserved |
|
| 0x02620318 |
0x0262031B |
4B |
Reserved |
|
| 0x0262031C |
0x0262031F |
4B |
Reserved |
|
| 0x02620320 |
0x02620323 |
4B |
Reserved |
|
| 0x02620324 |
0x02620327 |
4B |
Reserved |
|
| 0x02620328 |
0x0262032B |
4B |
MAINPLLCTL0 |
See Section 8.5 |
| 0x0262032C |
0x0262032F |
4B |
MAINPLLCTL1 |
| 0x02620330 |
0x02620333 |
4B |
DDR3PLLCTL0 |
See Section 8.6 |
| 0x02620334 |
0x02620337 |
4B |
DDR3PLLCTL1 |
| 0x02620338 |
0x0262033B |
4B |
Reserved |
|
| 0x0262033C |
0x0262033F |
4B |
Reserved |
|
| 0x02620340 |
0x02620343 |
4B |
SGMII_SERDES_CFGPLL |
See Section 9.2 |
| 0x02620344 |
0x02620347 |
4B |
SGMII_SERDES_CFGRX0 |
| 0x02620348 |
0x0262034B |
4B |
SGMII_SERDES_CFGTX0 |
| 0x0262034C |
0x0262034F |
4B |
Reserved |
| 0x02620350 |
0x02620353 |
4B |
Reserved |
| 0x02620354 |
0x02620357 |
4B |
Reserved |
| 0x02620358 |
0x0262035B |
4B |
PCIE_SERDES_CFGPLL |
| 0x0262035C |
0x0262035F |
4B |
Reserved |
| 0x02620360 |
0x02620363 |
4B |
Reserved |
|
| 0x02620364 |
0x02620367 |
4B |
Reserved |
| 0x02620368 |
0x0262036B |
4B |
Reserved |
| 0x0262036C |
0x0262036F |
4B |
Reserved |
| 0x02620370 |
0x02620373 |
4B |
Reserved |
| 0x02620374 |
0x02620377 |
4B |
Reserved |
| 0x02620378 |
0x0262037B |
4B |
Reserved |
| 0x0262037C |
0x0262037F |
4B |
Reserved |
| 0x02620380 |
0x02620383 |
4B |
Reserved |
| 0x02620384 |
0x02620387 |
8B |
Reserved |
|
| 0x026203B4 |
0x026203B7 |
4B |
Reserved |
|
| 0x026203B8 |
0x026203BB |
4B |
Reserved |
| 0x026203BC |
0x026203BF |
4B |
Reserved |
| 0x026203C0 |
0x026203C3 |
4B |
Reserved |
| 0x026203C4 |
0x026203C7 |
4B |
Reserved |
| 0x026203C8 |
0x026203CB |
4B |
Reserved |
| 0x026203CC |
0x026203CF |
4B |
Reserved |
| 0x026203D0 |
0x026203D3 |
4B |
Reserved |
| 0x026203D4 |
0x026203D7 |
4B |
Reserved |
| 0x026203D8 |
0x026203DB |
4B |
Reserved |
|
| 0x026203DC |
0x026203F7 |
28B |
Reserved |
|
| 0x026203F8 |
0x026203FB |
4B |
DEVSPEED |
See Section 4.3.19 |
| 0x026203FC |
0x026203FF |
4B |
Reserved |
|
| 0x02620400 |
0x02620403 |
4B |
PKTDMA_PRI_ALLOC |
See Section 5.4 |
| 0x02620404 |
0x02620467 |
100B |
Reserved |
|
| 0x02620468 |
0x0262057f |
280B |
Reserved |
|
| 0x02620580 |
0x02620583 |
4B |
PIN_CONTROL_0 |
See Section 4.3.20 |
| 0x02620584 |
0x02620587 |
4B |
PIN_CONTROL_1 |
See Section 4.3.21 |
| 0x02620588 |
0x0262058B |
4B |
EMAC_UPP_PRI_ALLOC |
See Section 5.4 |
4.3.1 Device Status Register
The Device Status Register depicts the device configuration selected upon a power-on reset by either the POR or RESETFULL pin. Once set, these bits will remain set until the next power-on reset. The Device Status Register is shown in Figure 4-1 and described in Table 4-3.
Figure 4-1 Device Status Register
| Reserved |
PCIESSEN |
PCIESSMODE [1:0] |
BOOTMODE[12:0] |
LENDIAN |
| R-0 |
R-x |
R/W-xx |
R/W-xxxxxxxxxxxx |
R-x(1) |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
(1) x indicates the bootstrap value latched via the external pin
Table 4-3 Device Status Register Field Descriptions
| Bit |
Field |
Description |
| 31-17 |
Reserved |
Reserved. Read only, writes have no effect. |
| 16 |
PCIESSEN |
PCIe module enable
- 0 = PCIe module disabled
- 1 = PCIe module enabled
|
| 15-14 |
PCIESSMODE[1:0] |
PCIe Mode selection pins
- 00b = PCIe in End-point mode
- 01b = PCIe in Legacy End-point mode (support for legacy INTx)
- 10b = PCIe in Root complex mode
- 11b = Reserved
|
| 13-1 |
BOOTMODE[12:0] |
Determines the bootmode configured for the device. For more information on bootmode, refer to Section 3.5 and see the Bootloader for the C66x DSP User's Guide (SPRUGY5) |
| 0 |
LENDIAN |
Device Endian mode (LENDIAN) — Shows the status of whether the system is operating in Big Endian mode or Little Endian mode.
- 0 = System is operating in Big Endian mode
- 1 = System is operating in Little Endian mode
|
4.3.2 Device Configuration Register
The Device Configuration Register is one-time writeable through software. The register is reset on all hard resets and is locked after the first write. The Device Configuration Register is shown in Figure 4-2 and described in Table 4-4.
Figure 4-2 Device Configuration Register (DEVCFG)
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-4 Device Configuration Register Field Descriptions
| Bit |
Field |
Description |
| 31-1 |
Reserved |
Reserved. Read only, writes have no effect. |
| 0 |
SYSCLKOUTEN |
SYSCLKOUT Enable
- 0 = No clock output
- 1 = Clock output enabled (default)
|
4.3.3 JTAG ID (JTAGID) Register Description
The JTAG ID register is a read-only register that identifies to the customer the JTAG/Device ID. For the device, the JTAG ID register resides at address location 0x0262 0018. The JTAG ID Register is shown in Figure 4-3 and described in Table 4-5.
Figure 4-3 JTAG ID (JTAGID) Register
| VARIANT |
PART NUMBER |
MANUFACTURER |
LSB |
| R-xxxxb |
R-1011 1001 0111 1010b |
0000 0010 111b |
R-1 |
| Legend: RW = Read/Write; R = Read only; -n = value after reset |
Table 4-5 JTAG ID Register Field Descriptions
| Bit |
Field |
Value |
Description |
| 31-28 |
VARIANT |
xxxxb |
Variant (4-Bit) value. |
| 27-12 |
PART NUMBER |
1011 1001 0111 1010b |
Part Number for boundary scan |
| 11-1 |
MANUFACTURER |
0000 0010 111b |
Manufacturer |
| 0 |
LSB |
1b |
This bit is read as a 1 for C6654 |
NOTE
The value of the VARIANT and PART NUMBER fields depend on the silicon revision. See the Silicon Errata for details.
4.3.4 Kicker Mechanism (KICK0 and KICK1) Register
The Bootcfg module contains a kicker mechanism to prevent any spurious writes from changing any of the Bootcfg MMR values. When the kicker is locked (which it is initially after power on reset), none of the Bootcfg MMRs are writable (they are only readable). On the C6654, the exceptions to this are the IPC registers such as IPCGRx and IPCARx. These registers are not protected by the kicker mechanism. This mechanism requires two MMR writes to the KICK0 and KICK1 registers with exact data values before the kicker lock mechanism is un-locked. See Table 4-2 for the address location. Once released, then all the Bootcfg MMRs having write permissions are writable (the read only MMRs are still read only). The first KICK0 data is 0x83e70b13. The second KICK1 data is 0x95a4f1e0. Writing any other data value to either of these kick MMRs will lock the kicker mechanism and block any writes to Bootcfg MMRs. To ensure protection of all Bootcfg MMRs, software must always re-lock the kicker mechanism after completing the MMR writes.
4.3.5 LRESETNMI PIN Status (LRSTNMIPINSTAT) Register
The LRSTNMIPINSTAT Register is created in Boot Configuration to latch the status of LRESET and NMI based on CORESEL. The LRESETNMI PIN Status Register is shown and described in the following tables.
Figure 4-4 LRESETNMI PIN Status Register (LRSTNMIPINSTAT)
| Reserved |
Reserved |
NMI0 |
Reserved |
Reserved |
LR0 |
| R, +0000 0000 |
R-0 |
WC,+0 |
R, +0000 0000 |
WC,+0 |
WC,+0 |
| Legend: R = Read only; -n = value after reset; |
Table 4-6 LRESETNMI PIN Status Register (LRSTNMIPINSTAT) Field Descriptions
| Bit |
Field |
Description |
| 31-18 |
Reserved |
Reserved |
| 17 |
Reserved |
Reserved |
| 16 |
NMI0 |
CorePac0 in NMI |
| 15-2 |
Reserved |
Reserved |
| 1 |
Reserved |
Reserved |
| 0 |
LR0 |
CorePac0 in Local Reset |
4.3.6 LRESETNMI PIN Status Clear (LRSTNMIPINSTAT_CLR) Register
The LRSTNMIPINSTAT_CLR Register is used to clear the status of LRESET and NMI based on CORESEL. The LRESETNMI PIN Status Clear Register is shown and described in the following tables.
Figure 4-5 LRESETNMI PIN Status Clear Register (LRSTNMIPINSTAT_CLR)
| Reserved |
Reserved |
NMI0 |
Reserved |
Reserved |
LR0 |
| R, +0000 0000 |
WC,+0 |
WC,+0 |
R, +0000 0000 |
WC,+0 |
WC,+0 |
| Legend: R = Read only; -n = value after reset; WC = Write 1 to Clear |
Table 4-7 LRESETNMI PIN Status Clear Register (LRSTNMIPINSTAT_CLR) Field Descriptions
| Bit |
Field |
Description |
| 31-18 |
Reserved |
Reserved |
| 17 |
Reserved |
Reserved |
| 16 |
NMI0 |
CorePac0 in NMI Clear |
| 15-2 |
Reserved |
Reserved |
| 1 |
Reserved |
Reserved |
| 0 |
LR0 |
CorePac0 in Local Reset Clear |
4.3.7 Reset Status (RESET_STAT) Register
The reset status register (RESET_STAT) captures the status of Local reset (LRx) for each of the cores and also the global device reset (GR). Software can use this information to take different device initialization steps, if desired.
- In case of Local reset: The LRx bits are written as 1 and GR bit is written as 0 only when the CorePac receives a local reset without receiving a global reset.
- In case of Global reset: The LRx bits are written as 0 and GR bit is written as 1 only when a global reset is asserted.
The Reset Status Register is shown and described in the following tables.
Figure 4-6 Reset Status Register (RESET_STAT)
| R, +1 |
R, + 000 0000 0000 0000 0000 0000 |
R,+0 |
R,+0 |
| Legend: R = Read only; -n = value after reset |
Table 4-8 Reset Status Register (RESET_STAT) Field Descriptions
| Bit |
Field |
Description |
| 31 |
GR |
Global reset status
- 0 = Device has not received a global reset.
- 1 = Device received a global reset.
|
| 30-2 |
Reserved |
Reserved. |
| 1 |
Reserved |
Reserved. |
| 0 |
LR0 |
CorePac0 reset status
- 0 = CorePac0 has not received a local reset.
- 1 = CorePac0 received a local reset.
|
4.3.8 Reset Status Clear (RESET_STAT_CLR) Register
The RESET_STAT bits can be cleared by writing 1 to the corresponding bit in the RESET_STAT_CLR register. The Reset Status Clear Register is shown and described in the following tables.
Figure 4-7 Reset Status Clear Register (RESET_STAT_CLR)
| RW, +0 |
R, + 000 0000 0000 0000 0000 0000 |
RW,+0 |
RW,+0 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-9 Reset Status Clear Register (RESET_STAT_CLR) Field Descriptions
| Bit |
Field |
Description |
| 31 |
GR |
Global reset clear bit
- 0 = Writing a 0 has no effect.
- 1 = Writing a 1 to the GR bit clears the corresponding bit in the RESET_STAT register.
|
| 30-2 |
Reserved |
Reserved. |
| 1 |
Reserved |
Reserved. |
| 0 |
LR0 |
CorePac0 reset clear bit
- 0 = Writing a 0 has no effect.
- 1 = Writing a 1 to the LR0 bit clears the corresponding bit in the RESET_STAT register.
|
4.3.9 Boot Complete (BOOTCOMPLETE) Register
The BOOTCOMPLETE register controls the BOOTCOMPLETE pin status. The purpose is to indicate the completion of the ROM booting process. The Boot Complete Register is shown and described in the following tables.
Figure 4-8 Boot Complete Register (BOOTCOMPLETE)
| R, + 0000 0000 0000 0000 0000 0000 |
RW,+0 |
RW,+0 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-10 Boot Complete Register (BOOTCOMPLETE) Field Descriptions
| Bit |
Field |
Description |
| 31-2 |
Reserved |
Reserved. |
| 1 |
Reserved |
Reserved |
| 0 |
BC0 |
CorePac0 boot status
- 0 = CorePac0 boot NOT complete
- 1 = CorePac0 boot complete
|
The BCx bit indicates the boot complete status of the corresponding core. All BCx bits will be sticky bits — that is they can be set only once by the software after device reset and they will be cleared to 0 on all device resets.
Boot ROM code will be implemented such that each core will set its corresponding BCx bit immediately before branching to the predefined location in memory.
4.3.10 Power State Control (PWRSTATECTL) Register
The PWRSTATECTL register is controlled by the software to indicate the power-saving mode. ROM code reads this register to differentiate between the various power saving modes. This register is cleared only by POR and will survive all other device resets. See the Hardware Design Guide for KeyStone Devices (SPRABI2) for more information. The Power State Control Register is shown in Figure 4-9 and described in Table 4-11.
Figure 4-9 Power State Control Register (PWRSTATECTL)
| GENERAL_PURPOSE |
HIBERNATION _MODE |
HIBERNATION |
STANDBY |
| RW, +0000 0000 0000 0000 0000 0000 0000 0 |
RW,+0 |
RW,+0 |
RW,+0 |
| Legend: RW = Read/Write; -n = value after reset |
Table 4-11 Power State Control Register (PWRSTATECTL) Field Descriptions
| Bit |
Field |
Description |
| 31-3 |
GENERAL_PURPOSE |
Used to provide a start address for execution out of the hibernation modes. See the Bootloader for the C66x DSP User's Guide (SPRUGY8). |
| 2 |
HIBERNATION_MODE |
Indicates whether the device is in hibernation mode 1 or mode 2.
- 0 = Hibernation mode 1
- 1 = Hibernation mode 2
|
| 1 |
HIBERNATION |
Indicates whether the device is in hibernation mode or not.
- 0 = Not in hibernation mode
- 1 = Hibernation mode
|
| 0 |
STANDBY |
Indicates whether the device is in standby mode or not.
- 0 = Not in standby mode
- 1 = Standby mode
|
4.3.11 NMI Event Generation to CorePac (NMIGRx) Register
NMIGRx registers are used for generating NMI events to the CorePac. The C6654 has only NMIGR0, which generates an NMI event to the CorePac. Writing a 1 to the NMIG field generates an NMI pulse. Writing a 0 has no effect and reads return 0 and have no other effect. The NMI Event Generation to CorePac Register is shown in Figure 4-10 and described in Table 4-12.
Figure 4-10 NMI Generation Register (NMIGRx)
| R, +0000 0000 0000 0000 0000 0000 0000 000 |
RW,+0 |
| Legend: RW = Read/Write; -n = value after reset |
Table 4-12 NMI Generation Register (NMIGRx) Field Descriptions
| Bit |
Field |
Description |
| 31-1 |
Reserved |
Reserved |
| 0 |
NMIG |
NMI pulse generation. Reads return 0
Writes:
- 0 = No effect
- 1 = Sends an NMI pulse to the CorePac
|
4.3.12 IPC Generation (IPCGRx) Registers
IPCGRx are the IPC interrupt generation registers to facilitate inter CorePac interrupts.
The C6654 has only IPCGR0. This register can be used by external hosts to generate interrupts to the CorePac. A write of 1 to the IPCG field of the IPCGRx register will generate an interrupt pulse to the CorePac.
This register also provides a Source ID facility by which up to 28 different sources of interrupts can be identified. Allocation of source bits to source processor and meaning is entirely based on software convention. The register field descriptions are given in the following tables. Virtually anything can be a source for these registers as this is completely controlled by software. Any master that has access to BOOTCFG module space can write to these registers. The IPC Generation Register is shown in Figure 4-11 and described in Table 4-13.
Figure 4-11 IPC Generation Registers (IPCGRx)
| 31 |
30 |
29 |
28 |
27 |
|
|
|
8 |
7 |
6 |
5 |
4 |
3 |
1 |
0 |
SRCS 27 |
SRCS 26 |
SRCS 25 |
SRCS 24 |
SRCS23 – SRCS4 |
SRCS3 |
SRCS2 |
SRCS1 |
SRCS0 |
Reserved |
IPCG |
| RW +0 |
RW +0 |
RW +0 |
RW +0 |
RW +0 (per bit field) |
RW +0 |
RW +0 |
RW +0 |
RW +0 |
R, +000 |
RW +0 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-13 IPC Generation Registers (IPCGRx) Field Descriptions
| Bit |
Field |
Description |
| 31-4 |
SRCSx |
Interrupt source indication. Reads return current value of internal register bit.
Writes:
- 0 = No effect
- 1 = Sets both SRCSx and the corresponding SRCCx.
|
| 3-1 |
Reserved |
Reserved |
| 0 |
IPCG |
Inter-DSP interrupt generation. Reads return 0.
Writes:
- 0 = No effect
- 1 = Creates an Inter-DSP interrupt.
|
4.3.13 IPC Acknowledgement (IPCARx) Registers
IPCARx are the IPC interrupt-acknowledgement registers to facilitate inter-CorePac core interrupts.
The C6654 has only IPCAR0. This register also provides a Source ID facility by which up to 28 different sources of interrupts can be identified. Allocation of source bits to source processor and meaning is entirely based on software convention. The register field descriptions are shown in the following tables. Virtually anything can be a source for these registers as this is completely controlled by software. Any master that has access to BOOTCFG module space can write to these registers. The IPC Acknowledgement Register is shown in Figure 4-12 and described in Table 4-14.
Figure 4-12 IPC Acknowledgement Registers (IPCARx)
| 31 |
30 |
29 |
28 |
27 |
|
|
|
8 |
7 |
6 |
5 |
4 |
3 |
|
0 |
SRCC 27 |
SRCC 26 |
SRCC 25 |
SRCC 24 |
SRCC23 – SRCC4 |
SRCC3 |
SRCC2 |
SRCC1 |
SRCC0 |
Reserved |
| RW +0 |
RW +0 |
RW +0 |
RW +0 |
RW +0 (per bit field) |
RW +0 |
RW +0 |
RW +0 |
RW +0 |
R, +0000 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-14 IPC Acknowledgement Registers (IPCARx) Field Descriptions
| Bit |
Field |
Description |
| 31-4 |
SRCCx |
Interrupt source acknowledgement. Reads return current value of internal register bit.
Writes:
- 0 = No effect
- 1 = Clears both SRCCx and the corresponding SRCSx
|
| 3-0 |
Reserved |
Reserved |
4.3.14 IPC Generation Host (IPCGRH) Register
The IPCGRH register facilitates interrupts to external hosts. Operation and use of the IPCGRH register is the same as for other IPCGR registers. The interrupt output pulse created by the IPCGRH register appears on device pin HOUT.
The host interrupt output pulse should be stretched. It should be asserted for 4 bootcfg clock cycles (CPU/6) followed by a deassertion of 4 bootcfg clock cycles. Generating the pulse will result in 8 CPU/6 cycle pulse blocking window. Write to IPCGRH with IPCG bit (bit 0) set will only generate a pulse if they are beyond 8 CPU/6 cycle period. The IPC Generation Host Register is shown in Figure 4-13 and described in Table 4-15.
Figure 4-13 IPC Generation Registers (IPCGRH)
| 31 |
30 |
29 |
28 |
27 |
|
|
|
8 |
7 |
6 |
5 |
4 |
3 |
1 |
0 |
SRCS 27 |
SRCS 26 |
SRCS 25 |
SRCS 24 |
SRCS23 – SRCS4 |
SRCS3 |
SRCS2 |
SRCS1 |
SRCS0 |
Reserved |
IPCG |
| RW +0 |
RW +0 |
RW +0 |
RW +0 |
RW +0 (per bit field) |
RW +0 |
RW +0 |
RW +0 |
RW +0 |
R, +000 |
RW +0 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-15 IPC Generation Registers (IPCGRH) Field Descriptions
| Bit |
Field |
Description |
| 31-4 |
SRCSx |
Interrupt source indication. Reads return current value of internal register bit.
Writes:
- 0 = No effect
- 1 = Sets both SRCSx and the corresponding SRCCx.
|
| 3-1 |
Reserved |
Reserved |
| 0 |
IPCG |
Host interrupt generation. Reads return 0.
Writes:
- 0 = No effect
- 1 = Creates an interrupt pulse on device pin (host interrupt/event output in HOUT pin)
|
4.3.15 IPC Acknowledgement Host (IPCARH) Register
IPCARH registers are provided to facilitate host DSP interrupt. Operation and use of IPCARH is the same as other IPCAR registers. The IPC Acknowledgement Host Register is shown in Figure 4-14 and described in Table 4-16.
Figure 4-14 IPC Acknowledgement Register (IPCARH)
| 31 |
30 |
29 |
28 |
27 |
|
|
|
8 |
7 |
6 |
5 |
4 |
3 |
|
0 |
SRCC 27 |
SRCC 26 |
SRCC 25 |
SRCC 24 |
SRCC23 – SRCC4 |
SRCC3 |
SRCC2 |
SRCC1 |
SRCC0 |
Reserved |
| RW +0 |
RW +0 |
RW +0 |
RW +0 |
RW +0 (per bit field) |
RW +0 |
RW +0 |
RW +0 |
RW +0 |
R, +0000 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-16 IPC Acknowledgement Register (IPCARH) Field Descriptions
| Bit |
Field |
Description |
| 31-4 |
SRCCx |
Interrupt source acknowledgement. Reads return current value of internal register bit.
Writes:
- 0 = No effect
- 1 = Clears both SRCCx and the corresponding SRCSx
|
| 3-0 |
Reserved |
Reserved |
4.3.16 Timer Input Selection Register (TINPSEL)
Timer input selection is handled within the control register TINPSEL. The Timer Input Selection Register is shown in Figure 4-15 and described in Table 4-17.
Figure 4-15 Timer Input Selection Register (TINPSEL)
| 15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
TINPH SEL7 |
TINPL SEL7 |
TINPH SEL6 |
TINPL SEL6 |
TINPH SEL5 |
TINPL SEL5 |
TINPH SEL4 |
TINPL SEL4 |
TINPH SEL3 |
TINPL SEL3 |
TINPH SEL2 |
TINPL SEL2 |
TINPH SEL1 |
TINPL SEL1 |
TINPH SEL0 |
TINPL SEL0 |
| RW, +1 |
RW, +0 |
RW, +1 |
RW, +0 |
RW, +1 |
RW, +0 |
RW, +1 |
RW, +0 |
RW, +1 |
RW, +0 |
RW, +1 |
RW, +0 |
RW, +1 |
RW, +0 |
RW, +1 |
RW, +0 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-17 Timer Input Selection Field Description (TINPSEL)
| Bit |
Field |
Description |
| 31-16 |
Reserved |
|
| 15 |
TINPHSEL7 |
Input select for TIMER7 high.
|
| 14 |
TINPLSEL7 |
Input select for TIMER7 low.
|
| 13 |
TINPHSEL6 |
Input select for TIMER6 high.
|
| 12 |
TINPLSEL6 |
Input select for TIMER6 low.
|
| 11 |
TINPHSEL5 |
Input select for TIMER5 high.
|
| 10 |
TINPLSEL5 |
Input select for TIMER5 low.
|
| 9 |
TINPHSEL4 |
Input select for TIMER4 high.
|
| 8 |
TINPLSEL4 |
Input select for TIMER4 low.
|
| 7 |
TINPHSEL3 |
Input select for TIMER3 high.
|
| 6 |
TINPLSEL3 |
Input select for TIMER3 low.
|
| 5 |
TINPHSEL2 |
Input select for TIMER2 high.
|
| 4 |
TINPLSEL2 |
Input select for TIMER2 low.
|
| 3 |
TINPHSEL1 |
Input select for TIMER1 high.
|
| 2 |
TINPLSEL1 |
Input select for TIMER1 low.
|
| 1 |
TINPHSEL0 |
Input select for TIMER0 high.
|
| 0 |
TINPLSEL0 |
Input select for TIMER0 low.
|
4.3.17 Timer Output Selection Register (TOUTPSEL)
The timer output selection is handled within the control register TOUTSEL. The Timer Output Selection Register is shown in Figure 4-16 and described in Table 4-18.
Figure 4-16 Timer Output Selection Register (TOUTPSEL)
| Reserved |
TOUTPSEL1 |
TOUTPSEL0 |
| R,+000000000000000000000000 |
RW,+00001 |
RW,+00000 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-18 Timer Output Selection Field Description (TOUTPSEL)
| Bit |
Field |
Description |
| 31-10 |
Reserved |
Reserved |
| 9-5 |
TOUTPSEL1 |
Output select for TIMO1
- 0x0: TOUTL0
- 0x1: TOUTH0
- 0x2: TOUTL1
- 0x3: TOUTH1
- 0x4: TOUTL2
- 0x5: TOUTH2
- 0x6: TOUTL3
- 0x7: TOUTH3
- 0x8: TOUTL4
|
- 0x9: TOUTH4
- 0xA: TOUTL5
- 0xB: TOUTH5
- 0xC: TOUTL6
- 0xD: TOUTH6
- 0xE: TOUTL7
- 0xF: TOUTH7
- 0x10 to 0x1F: Reserved
|
| 4-0 |
TOUTPSEL0 |
Output select for TIMO0
- 0x0: TOUTL0
- 0x1: TOUTH0
- 0x2: TOUTL1
- 0x3: TOUTH1
- 0x4: TOUTL2
- 0x5: TOUTH2
- 0x6: TOUTL3
- 0x7: TOUTH3
- 0x8: TOUTL4
|
- 0x9: TOUTH4
- 0xA: TOUTL5
- 0xB: TOUTH5
- 0xC: TOUTL6
- 0xD: TOUTH6
- 0xE: TOUTL7
- 0xF: TOUTH7
- 0x10 to 0x1F: Reserved
|
4.3.18 Reset Mux (RSTMUXx) Register
The software controls the Reset Mux block through the reset multiplex registers using RSTMUX0. This register islocated in Bootcfg memory space. The Reset Mux Register is shown in Figure 4-17 and described in Table 4-19.
Figure 4-17 Reset Mux Register RSTMUXx
| Reserved |
EVTSTATCLR |
Reserved |
DELAY |
EVTSTAT |
OMODE |
LOCK |
| R, +0000 0000 0000 0000 0000 00 |
RC, +0 |
R, +0 |
RW, +100 |
R, +0 |
RW, +000 |
RW, +0 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset; RC = Read only and write 1 to clear |
Table 4-19 Reset Mux Register Field Descriptions
| Bit |
Field |
Description |
| 31-10 |
Reserved |
Reserved |
| 9 |
EVTSTATCLR |
Clear event status
- 0 = Writing 0 has no effect
- 1 = Writing 1 clears the EVTSTAT bit
|
| 8 |
Reserved |
Reserved |
| 7-5 |
DELAY |
Delay cycles between NMI & local reset
- 000b = 256 CPU/6 cycles delay between NMI & local reset, when OMODE = 100b
- 001b = 512 CPU/6 cycles delay between NMI & local reset, when OMODE=100b
- 010b = 1024 CPU/6 cycles delay between NMI & local reset, when OMODE=100b
- 011b = 2048 CPU/6 cycles delay between NMI & local reset, when OMODE=100b
- 100b = 4096 CPU/6 cycles delay between NMI & local reset, when OMODE=100b (Default)
- 101b = 8192 CPU/6 cycles delay between NMI & local reset, when OMODE=100b
- 110b = 16384 CPU/6 cycles delay between NMI & local reset, when OMODE=100b
- 111b = 32768 CPU/6 cycles delay between NMI & local reset, when OMODE=100b
|
| 4 |
EVTSTAT |
Event status.
- 0 = No event received (Default)
- 1 = WD timer event received by Reset Mux block
|
| 3-1 |
OMODE |
Timer event operation mode
- 000b = WD timer event input to the reset mux block does not cause any output event (default)
- 001b = Reserved
- 010b = WD timer event input to the reset mux block causes local reset input to CorePac
- 011b = WD timer event input to the reset mux block causes NMI input to CorePac
- 100b = WD timer event input to the reset mux block causes NMI input followed by local reset input to CorePac. Delay between NMI and local reset is set in DELAY bit field.
- 101b = WD timer event input to the reset mux block causes device reset to C6654
- 110b = Reserved
- 111b = Reserved
|
| 0 |
LOCK |
Lock register fields
- 0 = Register fields are not locked (default)
- 1 = Register fields are locked until the next timer reset
|
4.3.19 Device Speed (DEVSPEED) Register
The Device Speed Register indicates the device speed grade. The Device Speed Register is shown in Figure 4-18 and described in Table 4-20.
Figure 4-18 Device Speed Register (DEVSPEED)
| Reserved |
DEVSPEED |
Reserved |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-20 Device Speed Register Field Descriptions
| Bit |
Field |
Description |
| 31 |
Reserved |
Reserved. Read only |
| 30-23 |
DEVSPEED |
Indicates the speed of the device (Read Only)
- 1xxx xxxxb = 850 MHz
- 01xx xxxxb = Reserved
- 001x xxxxb = Reserved
- 0001 xxxxb = Reserved
- 0000 1xxxb = Reserved
- 0000 01xxb = Reserved
- 0000 001xb = Reserved
- 0000 0001b = 850 MHz
- 0000 0000b = 850 MHz
|
| 22-0 |
Reserved |
Reserved. Read only |
4.3.20 Pin Control 0 (PIN_CONTROL_0) Register
The Pin Control 0 Register controls the pin muxing between GPIO[16:31] and TIMER / UART / SPI pins. The Pin Control 0 Register is shown in Figure 4-19 and described in Table 4-21.
Figure 4-19 Pin Control 0 Register (PIN_CONTROL_0)
| GPIO31_SPIDOUT_MUX |
GPIO30_SPIDIN_MUX |
GPIO29_SPICS1_MUX |
GPIO28_SPICS0_MUX |
GPIO27_UARTRTS1_MUX |
GPIO26_UARTCTS1_MUX |
GPIO25_UARTTX1_MUX |
GPIO24_UARTRX1_MUX |
| RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
| GPIO23_UARTRTS0_MUX |
GPIO22_UARTCTS0_MUX |
GPIO21_UARTTX0_MUX |
GPIO20_UARTRX0_MUX |
GPIO19_TIMO1_MUX |
GPIO18_TIMO0_MUX |
GPIO17_TIMI1_MUX |
GPIO16_TIMI0_MUX |
| RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
RW-0 |
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-21 Pin Control 0 Register Field Descriptions
| Bit |
Field |
Description |
| 31 |
GPIO31_SPIDOUT_MUX |
SPI or GPIO mux control
- 0 = SPIDOUT pin enabled
- 1 = GPIO31 pin enabled
|
| 30 |
GPIO30_SPIDIN_MUX |
SPI or GPIO mux control
- 0 = SPIDIN pin enabled
- 1 = GPIO30 pin enabled
|
| 29 |
GPIO29_SPICS1_MUX |
SPI or GPIO mux control
- 0 = SPICS1 pin enabled
- 1 = GPIO29 pin enabled
|
| 28 |
GPIO28_SPICS0_MUX |
SPI or GPIO mux control
- 0 = SPICS0 pin enabled
- 1 = GPIO28 pin enabled
|
| 27 |
GPIO27_UARTRTS1_MUX |
UART or GPIO mux control
- 0 = UARTRTS1 pin enabled
- 1 = GPIO27 pin enabled
|
| 26 |
GPIO26_UARTCTS1_MUX |
UART or GPIO mux control
- 0 = UARTCTS1 pin enabled
- 1 = GPIO26 pin enabled
|
| 25 |
GPIO25_UARTTX1_MUX |
UART or GPIO mux control
- 0 = UARTTX1 pin enabled
- 1 = GPIO25 pin enabled
|
| 24 |
GPIO24_UARTRX1_MUX |
UART or GPIO mux control
- 0 = UARTRX1 pin enabled
- 1 = GPIO24 pin enabled
|
| 23 |
GPIO23_UARTRTS0_MUX |
UART or GPIO mux control
- 0 = UARTRTS0 pin enabled
- 1 = GPIO23 pin enabled
|
| 22 |
GPIO22_UARTCTS0_MUX |
UART or GPIO mux control
- 0 = UARTCTS0 pin enabled
- 1 = GPIO22 pin enabled
|
| 21 |
GPIO21_UARTTX0_MUX |
UART or GPIO mux control
- 0 = UARTTX0 pin enabled
- 1 = GPIO21 pin enabled
|
| 20 |
GPIO20_UARTRX0_MUX |
UART or GPIO mux control
- 0 = UARTRX0 pin enabled
- 1 = GPIO20 pin enabled
|
| 19 |
GPIO19_TIMO1_MUX |
TIMER or GPIO mux control
- 0 = TIMO1 pin enabled
- 1 = GPIO19 pin enabled
|
| 18 |
GPIO18_TIMO0_MUX |
TIMER or GPIO mux control
- 0 = TIMO0 pin enabled
- 1 = GPIO18 pin enabled
|
| 17 |
GPIO17_TIMI1_MUX |
TIMER or GPIO mux control
- 0 = TIMI1 pin enabled
- 1 = GPIO17 pin enabled
|
| 16 |
GPIO16_TIMI0_MUX |
TIMER or GPIO mux control
- 0 = TIMI0 pin enabled
- 1 = GPIO16 pin enabled
|
| 15-0 |
Reserved |
Reserved |
4.3.21 Pin Control 1 (PIN_CONTROL_1) Register
The Pin Control 1 Register controls the pin muxing between uPP and EMIF16 pins. The Pin Control 1 Register is shown in Figure 4-20 and described in Table 4-22.
Figure 4-20 Pin Control 1Register (PIN_CONTROL_1)
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-22 Pin Control 1 Register Field Descriptions
| Bit |
Field |
Description |
| 31-1 |
Reserved |
Reserved |
| 0 |
UPP_EMIF_MUX |
uPP or EMIF16 mux control
- 0 = EMIF16 pins enabled
- 1 = uPP pins enabled
|
4.3.22 uPP Clock Source (UPP_CLOCK) Register
The uPP Clock Source Register controls whether the uPP transmit clock is internally or externally sourced. The uPP Clock Source Register is shown in Figure 4-21 and described in Table 4-23.
Figure 4-21 uPP Clock Source Register (UPP_CLOCK)
| Legend: R = Read only; RW = Read/Write; -n = value after reset |
Table 4-23 uPP Clock Source Register Field Descriptions
| Bit |
Field |
Description |
| 31-1 |
Reserved |
Reserved |
| 0 |
UPP_TX_CLKSRC |
uPP clock source selection
- 0 = from internal SYSCLK4 (CPU/3)
- 1 = from external UPP_2XTXCLK pin
|
4.4 Pullup/Pulldown Resistors
Proper board design should ensure that input pins to the device always be at a valid logic level and not floating. This may be achieved via pullup/pulldown resistors. The device features internal pullup (IPU) and internal pulldown (IPD) resistors on most pins to eliminate the need, unless otherwise noted, for external pullup/pulldown resistors.
An external pullup/pulldown resistor needs to be used in the following situations:
-
Device Configuration Pins: If the pin is both routed out and is not driven (in Hi-Z state), an external pullup/pulldown resistor must be used, even if the IPU/IPD matches the desired value/state.
-
Other Input Pins: If the IPU/IPD does not match the desired value/state, use an external pullup/pulldown resistor to pull the signal to the opposite rail.
For the device configuration pins (listed in Table 4-1), if they are both routed out and are not driven (in Hi-Z state), it is strongly recommended that an external pullup/pulldown resistor be implemented. Although, internal pullup/pulldown resistors exist on these pins and they may match the desired configuration value, providing external connectivity can help ensure that valid logic levels are latched on these device configuration pins. In addition, applying external pullup/pulldown resistors on the device configuration pins adds convenience to the user in debugging and flexibility in switching operating modes.
Tips for choosing an external pullup/pulldown resistor:
- Consider the total amount of current that may pass through the pullup or pulldown resistor. Make sure to include the leakage currents of all the devices connected to the net, as well as any internal pullup or pulldown resistors.
- Decide a target value for the net. For a pulldown resistor, this should be below the lowest VIL level of all inputs connected to the net. For a pullup resistor, this should be above the highest VIH level of all inputs on the net. A reasonable choice would be to target the VOL or VOH levels for the logic family of the limiting device; which, by definition, have margin to the VIL and VIH levels.
- Select a pullup/pulldown resistor with the largest possible value that can still ensure that the net will reach the target pulled value when maximum current from all devices on the net is flowing through the resistor. The current to be considered includes leakage current plus, any other internal and external pullup/pulldown resistors on the net.
- For bidirectional nets, there is an additional consideration that sets a lower limit on the resistance value of the external resistor. Verify that the resistance is small enough that the weakest output buffer can drive the net to the opposite logic level (including margin).
- Remember to include tolerances when selecting the resistor value.
- For pullup resistors, also remember to include tolerances on the DVDD rail.
For most systems:
- A 1-kΩ resistor can be used to oppose the IPU/IPD while meeting the above criteria. Users should confirm this resistor value is correct for their specific application.
- A 20-kΩ resistor can be used to compliment the IPU/IPD on the device configuration pins while meeting the above criteria. Users should confirm this resistor value is correct for their specific application.
For more detailed information on input current (II), and the low-level/high-level input voltages (VIL and VIH) for the C6654 device, see Section 7.3.
To determine which pins on the device include internal pullup/pulldown resistors, see Table 3-39.