ZHCSH87B September 2017 – February 2020 TMP461-SP
PRODUCTION DATA.
The Consecutive ALERT register (read address 22h, write address 22h) controls the number of out-of-limit temperature measurements required for ALERT to be asserted. Table 9 summarizes the values of the consecutive ALERT register. The number programmed in the consecutive ALERT applies to both the remote and local temperature results. When the number of times that the temperature result consecutively exceeds the high limit register value is equal to the value programmed in the consecutive ALERT register, ALERT is asserted. Similarly, the consecutive ALERT register setting is also applicable to the low-limit register.
REGISTER VALUE | NUMBER OF OUT-OF-LIMIT MEASUREMENTS REQUIRED TO ASSERT ALERT |
---|---|
01h | 1 (default) |
03h | 2 |
07h | 3 |
0Fh | 4 |