ZHCSP20 September 2022 TLV61070A
PRODUCTION DATA
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | SW | PWR | The switch pin of the converter. It is connected to the drain of the internal low-side power MOSFET and the source of the internal high-side power MOSFET. |
2 | GND | PWR | Ground pin of the IC |
3 | EN | I | Enable logic input. Logic high voltage enables the device. Logic low voltage disables the device and turns it into shutdown mode. |
4 | FB | I | Voltage feedback of adjustable output voltage |
5 | VOUT | PWR | Boost converter output |
6 | VIN | I | IC power supply input |