ZHCSDO6B May 2015 – September 2020 MSP430FG6425 , MSP430FG6426 , MSP430FG6625 , MSP430FG6626
PRODUCTION DATA
Table 8-1 explains how to compute the total current, ITOTAL, when the CTSD, along with associated modules, are used. See Section 8.8.14.2 for a similar table for the OA. A "yes" means it must be included in computing ITOTAL. Here is an example current calculation for CTS16D in rail-to-rail input mode (CTSD16RRI = 1) using the internal reference (CTSD16REFS = 1) and OA0 and OA1 enabled in rail-to-rail input modes, OARRI = 1.
As an example, assume that the application uses the CTS16D in rail-to-rail input mode (CTSD16RRI = 1) with the internal reference (CTSD16REFS = 1) and OA0 and OA1 are enabled in rail-to-rail input modes, OARRI = 1. The total current, ITOTAL, would be computed as follows:
| USE CASE NAME | USE CASE DETAILS | ICTSD16 | ICTSD16CLK (1) | ICP (2) | IREFBG (3) | IREF (4) |
|---|---|---|---|---|---|---|
| CTSD16 | yes | yes | no | yes if CTSD16REFS = 1 no if CTSD16REFS = 0 |
yes | |
| CTSD16 rail-to-rail inputs | CTSD16RRI = 1 | yes | yes | yes | yes if CTSD16REFS = 1 no if CTSD16REFS = 0 |
yes |
Section 8.8.11.2 lists the characteristics of the CTSD16 external voltage reference.