ZHCSO29 July 2021 LP5890
PRODUCTION DATA
Each memory BANK contains the frame-image grayscale data of all the 32 lines. Each line comprises sixteen 48-bit-width memory units. Each memory unit contains the grayscale data of the corresponding R/G/B channels.
Depending on the number of scan lines set in SCAN_NUM (FC0 bit 20 to bit 16), the total number of memory units that must be written in one BANK is: 48 × the number of scan lines. For example, if the number of scan lines is set to 32, then 1536 (32 × 48 = 1536) memory units must be written during each frame period.
Figure 8-23 shows the detailed memory structure of the LP5890 device.
Figure 8-23 LP5890 Memory-unit Structure