ZHCSE36E August 2015 – September 2024 LMK03328
PRODUCTION DATA
The RAMDAT register provides read and write access to the SRAM that forms part of the on-chip EEPROM module.
| Bit # | Field | Type | Reset | EEPROM | Description |
|---|---|---|---|---|---|
| [7:0] | RAMDAT[7:0] | RW | 0x00 | N | RAM Read/Write Data. The first time an I2C read or write transaction accesses the RAMDAT register address, either because the address is explicitly targeted or because the address is auto-incremented, a read transaction returns the RAM data located at the address specified by the MEMADR register and a write transaction causes the current I2C data to be written to the address specified by the MEMADR register. Any additional accesses which are part of the same transaction causes the RAM address to be incremented and a read or write access occurs at the next SRAM address. The I2C address is no longer auto-incremented (that is, the I2C address is locked to the RAMDAT register after the first access). Access to the RAMDAT register terminates at the end of the current I2Cs transaction. |