ZHCS747D January 2012 – September 2021 LMK01801
PRODUCTION DATA
These bits individually select the analog delay block for use with CLKout12 or CLKout13. It is not required for both outputs of a clock output group to use analog delay, but if both outputs do select the analog delay block, then the analog delay will be the same for each output. When neither clock output uses analog delay, the analog delay block is powered down.
| R5[13] | R5[14] | STATE |
|---|---|---|
| 0 | 0 | Analog delay powered down |
| 0 | 1 | Analog delay on CLKout13 |
| 1 | 0 | Analog delay on CLKout12 |
| 1 | 1 | Analog delay on both CLKouts |