ZHCSJ02A november 2018 – august 2020 DRV5057
PRODUCTION DATA
Figure 8-3 shows the magnetic field present at the sensor as the magnet passes by as described in Figure 8-2. The change in distance from the trough to the peak is approximately the length (thickness) of the magnet. B changes based on the strength of the magnet and how close the magnet is to the sensor.
Figure 8-3 Magnetic Field vs Distance